JAJST77 July 2024 TPS551892-Q1
PRODUCTION DATA
The TPS551892-Q1 outputs a voltage at the CDC pin proportional to the sensed voltage across a output current sensing resistor between the ISP pin and the ISN pin. Equation 6 shows the exact voltage at the CDC pin related to the sensed output current.

To compensate the voltage droop across a cable from the output of the USB port to its powered device, the TPS551892-Q1 can lift its output voltage in proportion to the load current by placing a resistor between the CDC pin and AGND pin.
The output voltage rises in proportion to the current sourcing from the CDC pin through the resistor at the CDC pin. It is recommended to use 100kΩ resistance for the up resistor of the feedback resistor divider. Equation 7 shows the output voltage rise related to the sensed output current, the resistance at the CDC pin, and the up resistor of the output voltage feedback resistor divider.

where
When RFB_UP is 100kΩ, the output voltage rise versus the sensed output current and the resistor at the CDC pin is shown in Figure 6-6.
Figure 6-6 Output Voltage Rise versus Output Current