JAJSUG2A May 2024 – October 2024 BQ25856-Q1
PRODUCTION DATA
In some applications, a regulated voltage is required when the adapter power is removed. The BQ25856 integrates an auto-reverse function which provides a regulated voltage using the buck-boost converter in reverse direction once the input power is removed.
When enabled by setting the AUTO_REV register bit to 1, Auto Reverse mode can be used to provide a regulated voltage immediately after the input power is removed. The device transitions to reverse mode when the input falls below the ACUV threshold.
The Auto Reverse mode operation will be automatically enabled if the following conditions are valid:
While the Auto reverse mode is active, the device sets the REVERSE_STAT bit to 1. Host can disable the Auto reverse operation at any time by setting EN_AUTO_REV = 0 and EN_REV = 0 with an I2C command.