JAJSVD9 August 2024 BQ25758S
PRODUCTION DATA
The power supply for the device is any DC voltage source within the specified input range. The supply should also be capable of supplying sufficient current based on the programmed input current limit. The input supply should be bypassed with a combination of electrolytic and ceramic capacitors to avoid ringing due to the parasitic impedance of the connecting cables.
When device is operating in the reverse direction, the supply at the OUTPUT should follow the same recommendations as the input supply mentioned above.