JAJSVI4 October 2024 ADS127L21B
PRODUCTION DATA
Normal-mode rejection ratio (NMRR) specifies the ability of the ADC to reject normal-mode input signals at specific frequencies. These frequencies are typically expressed at 50Hz and 60Hz input frequencies. Normal-mode rejection is uniquely determined by the frequency response of the digital filter. In this case, nulls in the frequency response of the low-latency sinc3 and sinc4 filters located at 50Hz and 60Hz provide rejection at these frequencies.