JAJU678 January 2019
To download the firmware to the board, an XDS110 USB Debug Probe is required. The XDS110 USB Debug probe can come as a standalone programmer or from most TI LaunchPad™ development kits. For this design, we configured a TI LaunchPad to work as an XDS110 USB Debug probe along with the 10-pin ribbon cable that comes with the Launchpad (see Figure 10).
After configuring the LaunchPad, he designer can click on the Debug button shown in to download the firmware using CCSv8.2. Figure 11.