SBOU302A June 2023 – December 2023 INA740B , INA745A , INA745B , INA780B
This section describes the circuitry of the input signal path.
The EZShunt digital power monitors provide an integrated shunt (IS+ to IS-), Kelvin sense connections (SH+ to SH-), and ADC differential input pins (IN+ and IN-). Thus, these devices have the ability to implement differential input filtering if desired in between the SH+/SHI pins and the IN+/IN- pins; however, to maximize thermal capability the input filters cannot be added to the EVM as of now because Kelvin sense pins are electrically tied to internal ADC input pins. If current filtering is necessary, then a user can configure longer conversion times and/or higher number of averages for the current register.
The VBUS pin is also electrically tied to the IS+ net to also optimize thermal performance.
All that is necessary to provide an input signal to U1 is to simply insert the IS+ (MP1) and IS- (MP2) nets in-series of the EVM with any current carrying wire provided the current and voltage are within EVM limits.