SBVU080 September 2023
Figure 4-2 through Figure 4-9 illustrate the board layout for the TRKRLDOEVM-119 PCB.
The TRKRLDOEVM-119 dissipates power, which can cause some components to experience an increase in temperature. The populated tracker LDO and pulsed resistors R11, R12, R13, R14, and R15 are most at risk of raising the junction temperature during normal operation. The LDO can become hot to the touch during normal operation; see the thermal impedance discussion in the populated tracker LDO data sheet.