SFFS817 March   2024 SN74AXC1T45-Q1

 

  1.   1
  2.   Trademarks
  3. 1Overview
  4. 2Functional Safety Failure In Time (FIT) Rates
    1. 2.1 SC70 Package
    2. 2.2 SON Package
  5. 3Failure Mode Distribution (FMD)
  6. 4Pin Failure Mode Analysis (Pin FMA)

Pin Failure Mode Analysis (Pin FMA)

This section provides a failure mode analysis (FMA) for the pins of the SN74AXC1T45-Q1 (SC70 and SON packages). The failure modes covered in this document include the typical pin-by-pin failure scenarios:

Table 4-2 through Table 4-6 also indicate how these pin conditions can affect the device as per the failure effects classification in Table 4-1.

Table 4-1 TI Classification of Failure Effects
ClassFailure Effects
APotential device damage that affects functionality
BNo device damage, but loss of functionality
CNo device damage, but performance degradation
DNo device damage, no impact to functionality or performance

Pin Diagram shows the SN74AXC1T45-Q1 pin diagram. For a detailed description of the device pins, see the Pin Configuration and Functions section in the SN74AXC1T45-Q1 data sheet.

GUID-72EDE79A-34A9-457B-99AA-5A1B86B9B9BD-low.gifFigure 4-1 Pin Diagram

Following are the assumptions of use and the device configuration assumed for the pin FMA in this section:

Table 4-2 Pin FMA for Device Pins Short-Circuited to Ground
Pin NamePin No.Description of Potential Failure Effect(s)Failure Effect Class
VCCA1GND short to VCC, device will be bypassed; may cause system damage, but not device damageB
GND2Normal OperationD
A3If configured as an output then damage is possible. If configured as input, no damage, but output will not switchA
B4If configured as an output then damage is possible. If configured as input, no damage, but output will not switchA
DIR5Direction control will fix B --> A directionB
VCCB6GND short to VCC, device will be bypassed - may cause system damage, but not device damageB
Table 4-3 Pin FMA for Device Pins Open-Circuited
Pin NamePin No.Description of Potential Failure Effect(s)Failure Effect Class
VCCA1Device will not be poweredB
GND2Device will not be poweredB
A3If configured as output, normal operation. If configured as input, no damage, but output will not switchB
B4If configured as output, normal operation. If configured as input, no damage, but output will not switchB
DIR5Direction control will fix B --> A directionB
VCCB6Device will not be poweredB
Table 4-4 Pin FMA for Device Pins Short-Circuited to Adjacent Pin
Pin NamePin No.Shorted toDescription of Potential Failure Effect(s)Failure Effect Class
VCCA1GNDGND short to VCC, device will be bypassed; may cause system damage, but not device damageB
GND2AIf A is configured as an output then damage is possible. If configured as input, output will be fixed LOWA
A3BBoth bits will have the same value always, but could have bus contention during transitions that may cause high currentA
B4DIRIf DIR is LOW, B will be an input and drive the output LOW. If DIR is HIGH, B will be an output and damage is possible based on state of A.A
DIR5VCCBIf VCCB>VCCA, DIR will fix B --> A direction OR if VCCB<VCCA, input could be inappropriate logic level potentially causing damageA
VCCB6VCCAVCCB short to VCCA, device will be bypassed; may cause system damage, but not device damageB
Table 4-5 Pin FMA for Device Pins Short-Circuited to VCCA
Pin NamePin No.Description of Potential Failure Effect(s)Failure Effect Class
VCCA1Normal OperationD
GND2GND short to VCC, device will be bypassed; may cause system damage, but not device damageB
A3If configured as an output then damage is possible. If configured as input, no damage, but output will not switchA
B4If configured as an output then damage is possible. If configured as input, damage is possible if VIH/VIL not metA
DIR5Direction control will fix A --> B directionB
VCCB6VCCA short to VCCB, device will be bypassed; may cause system damage, but not device damageB
Table 4-6 Pin FMA for Device Pins Short-Circuited to VCCB
Pin NamePin No.Description of Potential Failure Effect(s)Failure Effect Class
VCCA1VCCB short to VCCA, device will be bypassed; may cause system damage, but not device damageB
GND2GND short to VCC, device will be bypassed; may cause system damage, but not device damageB
A3If configured as an output then damage is possible. If configured as input, damage is possible if VIH/VIL not metA
B4If configured as an output then damage is possible. If configured as input, no damage, but output will not switchA
DIR5If VCCB>VCCA, DIR will fix B --> A direction OR if VCCB is less than VCCA, input could be inappropriate logic level potentially causing damageA
VCCB6Normal OperationD