SLAAE59 may 2023 AFE539A4
| Register Address |
Register Name |
Value | Description |
|---|---|---|---|
| 0x27 | STATE-MACHINE-CONFIG0 | 0x0003 | [15:3] 0x0 Don’t care |
| [2] 0b0: Do not abort state machine | |||
| [1] 0b1: Start state machine. Must be enabled in bit 0 as well | |||
| [0] 0b1: Enable state machine. Note: State machine must be disabled when configuring registers; enable state machine before saving to NVM. | |||
| 0x1F | COMMON-CONFIG | 0x1249 | [15] 0b0: Write 0b1 to set window-comparator output to a latching output |
| [14] 0b0: Write 0b1 to lock device. Unlock by writing 0b0101 to DEVUNLOCK field in the COMMON-TRIGGER register | |||
| [13] 0b0: Write 0b1 to set fault-dump read enable at address 0x01 | |||
| [12] 0b0: Write 0b1 to enable the internal reference | |||
| [11:10] 0b11: Power down VOUT3 | |||
| [9] 0b1: Power down IOUT3 | |||
| [8:7] 0b11: Power down VOUT2 | |||
| [6] 0b1: Power down IOUT2 | |||
| [5:4] 0b11: Powers-down VOUT1 | |||
| [3] 0b1: Power down IOUT1 | |||
| [2:1] 0b11: Power down VOUT0 | |||
| [0] 0b0: Power up IOUT0 | |||
| 0x02 | COMMON-TRIGGER | 0x0002 | [15:12] 0b000: Write 0b0101 to unlock the device |
| [11:8] 0b0000: Write 0b1010 to trigger a POR reset | |||
| [7] 0b0: Write 0b1 to trigger LAFE operation if the respective SYNCCONFIG-X bit in the AFE-X-FUNC-CONFIG register is 1 | |||
| [6] 0b0: Write 0b1 to set the AFE registers and outputs to zero-code or mid-code based on the respective CLR-SEL-X bit in the AFE-XFUNC-CONFIG register | |||
| [5] 0b0: Don’t care | |||
| [4] 0b0: Write 0b1 to trigger fault-dump sequence | |||
| [3] 0b0: Write 0b1 to trigger PROTECT function | |||
| [2] 0b0: Write 0b1 to read one row of NVM for fault-dump | |||
| [1] 0b1: Write 0b1 to store applicable register settings to the NVM | |||
| [0] 0b0: Write 0b1 to reload applicable registers with existing NVM settings |
| Register Address |
Register Name |
Value | Description |
|---|---|---|---|
| 0x03 | DAC-0-VOUT-CMP-CONFIG | 0x1405 | [15:13] 0x0: Don’t care |
| [12:10] 0b101: Set gain to 4 ×, use internal reference | |||
| [9:5] 0x0: Don’t care | |||
| [4] 0b0: Set OUTx pin to push-pull | |||
| [3] 0b0: Generate comparator output but consume internally | |||
| [2] 0b1: FB pin input has finite impedance | |||
| [1] 0b0: Do not invert the comparator output | |||
| [0] 0b1: Enable comparator mode. Current-output must be in power down | |||
| 0x09 | DAC-1-VOUT-CMP-CONFIG, | 0x800 | [15:13] 0x0: Don’t care |
| [12:10] 0b010: Set gain to 1.5 ×, use internal reference | |||
| [9:5] Don’t care | |||
| [4] 0b0: Set OUTx pin to push-pull | |||
| [3] 0b0: Generate comparator output but consume internally | |||
| [2] 0b0: FB pin has high impedance | |||
| [1] 0b0: Do not invert the comparator output | |||
| [0] 0b0: Disable comparator mode. | |||
| 0x0F | DAC-2-VOUT-CMP-CONFIG | 0x0403 | [15:13] Don’t care |
| [12:10] 0b001: Set gain to 1 ×, use VDD as reference | |||
|
[9:5] 0x0: Don’t care |
|||
| [4] 0b0: Set OUTx pin to push-pull | |||
| [3] 0b0: Generate comparator output but consume internally | |||
| [2] 0b0: FB pin has high impedance | |||
| [1] Invert comparator output | |||
| [0] 0b1: Enable comparator mode. Current-output must be in power down | |||
| 0x15 | DAC-3-VOUT-CMP-CONFIG | 0x1405 | [15:13] 0x0: Don’t care |
| [12:10] 0b101: Set gain to 4 ×, use internal reference | |||
| [9:5] Don’t care | |||
| [4] 0b0: Set OUTx pin to push-pull | |||
| [3] 0b0: Generate comparator output but consume internally | |||
| [2] 0b1: FB pin has finite impedance | |||
| [1] 0b0: Do not invert comparator output | |||
| [0] 0b1: Enable comparator mode. Current-output must be in power down |
| Register Address |
Register Name |
Value | Description |
|---|---|---|---|
| 0x20 | SRAM_DATA_32 | 0xE1C0 | [15:6] 0b1110000111: Input the maximum voltage output for the AFE. Value provided is for 1.6 V |
| [5:0] 0x0: Don’t care | |||
| 0x21 | SRAM_DATA_33 | 0x70C0 | [15:6] 0b:0111000011: Configure the minimum output of the AFE |
| [5:0] 0x0: Don’t care | |||
| 0x22 | SRAM_DATA_34 | 0x02DA | [15:10] 0x0: Don’t care |
| [9:0] 0b:001011011010: Configure the setpoint value. Setpoint is the value the ADC is compared to by the PI controller | |||
| 0x23 | SRAM_DATA_35 | 0x007F | [15:0] 0b:0000000001111111 Configure the proportional gain (KP) value for the PI controller |
| 0x24 | SRAM_DATA_36 | 0x8000 | [15:6] 0b1000000000000000: Set the threshold value of comparator channel 2 |
| [5:0] 0x0: Don’t care | |||
| 0x25 | SRAM_DATA_37 | 0x2FF | [15:12] 0x0: Don’t care |
| [11:2] 0b0010111111: Configure the common-mode value. The common-mode value is present at the PI output when KP and KI are zero | |||
| [1:0] 0x0: Don’t care | |||
| 0x26 | SRAM_DATA_38 | 0x0007 | [15:0] 0b0000000000000011: Select the integral gain value for the PI Controller. Setting this value to 0 disables KI |
| 0x27 | SRAM_DATA_39 | 0x0002 | [15:6] 0b0000000000: Safe-Output value |
| [5:2] 0x0: Don’t care | |||
| [1] 0b1: Select a finite-impedance input for ADC0 | |||
| [0] 0b0: Configure the loop polarity of the PI controller |