SLAAEB8A February   2024  – August 2025 MSPM0G1106 , MSPM0G1107 , MSPM0G1505 , MSPM0G1506 , MSPM0G1507 , MSPM0G1518 , MSPM0G1519 , MSPM0G3106 , MSPM0G3106-Q1 , MSPM0G3107 , MSPM0G3107-Q1 , MSPM0G3505 , MSPM0G3505-Q1 , MSPM0G3506 , MSPM0G3506-Q1 , MSPM0G3507 , MSPM0G3507-Q1 , MSPM0G3518 , MSPM0G3518-Q1 , MSPM0G3519 , MSPM0G3519-Q1

 

  1.   1
  2. 1Description
  3. 2Required Peripherals
  4. 3Design Steps
  5. 4Design Considerations
  6. 5Software Flow Chart
  7. 6Application Code
  8. 7Additional Resources
  9. 8E2E
  10. 9Revision History
  11.   Trademarks

Design Considerations

  1. Input signal bandwidth: The bandwidth of the signal that must be resolved determines the ADC sampling frequency and the amount of data the code must process.
  2. ADC reference voltage: The ADC reference voltage must be selected so the signal amplitude can be fully captured with good resolution.
  3. Filter order: Every increase in filter order is another set of operations the user must perform per each sample. This increases the overall processing time between samples and limits the amount of other processes the user can perform. The result is an increase in filter rejection and increased resolution of the desired signal.