SLAAES6A February 2025 – August 2025 MSPM0C1105 , MSPM0C1106 , MSPM0G3507 , MSPM0H3216
This application makes use of the TI System Configuration Tool (SysConfig) graphical interface to generate the configuration code of the device peripherals. Using a graphical interface to configure the device peripherals streamlines the application prototyping process.
The code for what is described in Figure 5-2 is found in the beginning of main() in the i2c_to_spi_bridge.c file.