SLAU358Q September 2011 – October 2019
Determines if the selected address space can be used for flash, FRAM, or OTP programming.
Syntax
LONG WINAPI MSPGANG_Flash_valid_addr(LONG dest, LONG start_addr, LONG size );
Arguments
| LONG dest | Spare – not used |
| LONG start_addr | Memory region start address |
| LONG size | Number of bytes of memory region to be validated |
Result
| LONG | ERR_NONE (0) if address is programmable |
| Error code otherwise |