SLAU892A March 2023 – June 2024
The AFE11612EVM GUI incorporates interactive functions that help configure an individual AFE11612-SEP device using I2C or SPI communication. These functions are built into several GUI pages, as shown in the following subsections. The menu bar on the far left of the GUI allows the user to switch between pages. The menu bar displays the High Level Configuration page with DACs, ADCs, Alarms and GPIO + Temp subpages, as well as the Low Level Configuration page.
Before using the GUI, see the AFE11612-SEP device data sheet for detailed programming instructions.