SLUAAN9 February   2023 BQ769142 , BQ76942 , BQ76952 , BQ76972 , ISO1640 , LM5168

 

  1.   Abstract
  2.   Trademarks
  3. 1Introduction
  4. 2Stacked AFE Communication
    1. 2.1 Data Communications
    2. 2.2 Control Signals
  5. 3High-Side N-Channel MOSFET
    1. 3.1 Discharge MOSFET Turn On and Off Processes
    2. 3.2 PACK Port High Voltage
    3. 3.3 Quickly Turning Off the Discharge MOSFET
  6. 4Current Consumption of Stacked Groups
  7. 5Summary
  8. 6References

PACK Port High Voltage

Energy recovery when braking is a requirement for some motor-driving applications. If the battery is fully charged and both charge and discharge MOSFETs are off, the PACK side can have a high voltage, damaging the BQ769x2 if the PIN voltage is higher than 85 V. One easy way to block high voltage is to add a series diode D29 between the discharge MOSFET and TOP_DSG, but the diode also blocks the sink current to turn off discharge MOSFET. A resister R166 is connected in parallel with D29 to supply a current path to turn on Q49 when turning off the discharge MOSFET. D20 and R155 protect TOP_LD voltage over the maximum limitations of the top BQ769x2. D20 is also helpful to limit the TOP_DSG voltage because the DSG pin is always driven toward LD pin when turning the discharge MOSFET off. For the other high-voltage pins of both the top BQ769x2 and bottom BQ769x2, the Zeners and resisters are always helpful to limit the voltages within the absolute maximum values. But if these high-voltage pins are used for voltage measurement, further calibrations are normally required to secure good accuracy with the protective Zeners and resisters.