SLUAAX5 August   2024 BQ25750 , BQ40Z80 , MSPM0C1105 , MSPM0C1106 , MSPM0H3216 , MSPM0L1306

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2The Role of MCU in Smart Battery System
  6. 3Application Example Using BQ25750, BQ40z80, and MSPM0L1306
    1. 3.1 Gauge Setup
    2. 3.2 Charger Setup
    3. 3.3 MCU Setup
    4. 3.4 Communication Protocol
    5. 3.5 MCU Code Example
    6. 3.6 Data Collected
  7. 4Summary
  8. 5References

Data Collected

All the data collected was using the BQ40Z80 device, which follows the SBS guidelines, BQ25750 device with the I2C protocol, and MSPM0L1306 in between to translate.

The MCU polling the gauge is shown below.


 Transmission
                                        of Gauge Data to MCU through SMBus

Figure 3-10 Transmission of Gauge Data to MCU through SMBus

The SMBus structure observed follows the structure in Section 3.4. Also note that the data received is little endian. Charging Voltage: 0x6018 = 24600mV and Charging Current: 0x0866 = 2150mA. Note: This is before the gauge settings were changed to what is shown in Figure 3-2.

The MCU sending ChargingVoltage() and ChargingCurrent() to the charger is shown below.


 Transmission
                                        of Charger Data from MCU through I2C

Figure 3-11 Transmission of Charger Data from MCU through I2C

The I2C structure observed follows the structure in Section 3.4. Also note that the data transmitted is little endian. 24600mV ChargingVoltage() is scaled to 31 = 0x001F for the charger FB regulation target (following the logic in MCU Code Example) and charging current: 2150mA is scaled to 172 = 0x00AC. The address registers for the voltage and current are 0x00 and 0x02, respectively.

The complete charging profile can be seen below.


 Charging
                                        Profile Using the MCU

Figure 3-12 Charging Profile Using the MCU

Figure 3-12 illustrates the test result using test set up discussed in the previous section. The result follows the gauge setting detailed in Table 3-1 and charge profile in Figure 3-1. Charge current is first regulated to the charging current at low voltage setting. Once the battery voltage reaches the Medium Voltage Threshold setting, charge current is increased to charging current at medium voltage. Then, current drops to charging current at high voltage once the battery voltage is increased to High Voltage Threshold. Then, the charger enters constant voltage mode once the battery reaches the Max Charge Voltage. In constant voltage mode, the current tapers until the current reaches Termination current. The termination in this application is handled by the charger because, once the charger reaches termination current, the charger disables the charge. The termination can by handled by the gauge and MCU if needed, which can be done by disabling the enable termination bit in BQ25750.

Note: The PFM was disabled according data sheet of BQ25750 since the termination current was below 2A and the watchdog was disabled as the PFM was not needed.