SLUUBT4B June   2018  – June 2025 BQ40Z80

 

  1.   1
  2.   Description
  3.   Features
  4.   4
  5. 1Evaluation Module Overview
    1. 1.1 Introduction
    2. 1.2 Kit Contents
    3. 1.3 Ordering Information
    4. 1.4 BQ40Z80 and BQ771807 Circuit Module Performance Specification Summary
  6. 2Hardware
    1. 2.1 BQ40Z80EVM Quick Start Guide
      1. 2.1.1 Items Needed for EVM Setup and Evaluation
      2. 2.1.2 Software Installation
      3. 2.1.3 EVM Connections
      4. 2.1.4 Update Firmware
    2. 2.2 Battery Management Studio
      1. 2.2.1 Registers Screen
      2. 2.2.2 Setting Programmable bq40z80 Options
      3. 2.2.3 Calibration Screen
        1. 2.2.3.1 Voltage Calibration
        2. 2.2.3.2 Temperature Calibration
        3. 2.2.3.3 Current Calibration
      4. 2.2.4 Chemistry Screen
      5. 2.2.5 Firmware Screen
        1. 2.2.5.1 Programming the Flash Memory
        2. 2.2.5.2 Exporting the Flash Memory
      6. 2.2.6 Advanced Comm SMB Screen
  7. 3Hardware Design Files
    1. 3.1 bq40z80EVM Circuit Module Schematic
      1. 3.1.1 Precharge
      2. 3.1.2 Predischarge
      3. 3.1.3 LED Control
      4. 3.1.4 Emergency Shutdown
      5. 3.1.5 Testing Fuse-Blowing Circuit
    2. 3.2 Circuit Module Physical Layouts
      1. 3.2.1 Board Layout
      2. 3.2.2 bq40z80RevA Schematic
    3. 3.3 bq40z80EVM Bill of Materials
  8. 4Additional Information
    1. 4.1 Trademarks
  9. 5Related Documentation from Texas Instruments
  10. 6Revision History

Registers Screen

Run Battery Management Studio from the Start | Programs | Texas Instruments | Battery Management Studio menu sequence, or the Battery Management Studio shortcut. The Registers screen (see Figure 2-2) appears. The Registers section contains parameters used to monitor gauging. The Bit Registers section provides bit level picture of status and fault registers. A green flag indicates that the bit is 0 (low state) and a red flag indicates that the bit is 1 (high state). Data begins to appear once the Refresh (single-time scan) button is selected, or scans continuously if the Scan button is selected.

BQ40Z80EVM-020 Registers ScreenFigure 2-2 Registers Screen

The Battery Management Studio program provides a logging function which logs the values that are selected by the Log check boxes located beside each parameter in the Register section. To enable this function, select the Log button; this causes the Scan button to be selected. When logging is stopped, the Scan button is still selected and has to be manually deselected.

The Log Interval can be set by opening a Watch tab, and using the pull-down at the far right to select the desired Log Interval in milli-seconds.