SLUUC37D July 2019 – June 2025
The software provides a command API and drivers that are capable of implementing the examples provided in BQ79616-Q1 Software Design Reference.
The example code only provides a control interface to the BQ79616-Q1 and does not provide any other communications interface to the outside world. The customer is expected to develop their own communication implementation. Examples of communications interfaces available to the TMS570 are SPI, CAN, or UART. For the TMS570 example code, UART is the communication protocol used between the microcontroller and BQ79616-Q1 device.
This firmware provided with this application note provides source code examples of the command sequences described in the BQ79616-Q1 Software Design Reference.
Importing a project into Code Composer Studio™:
C:\ti\bq79616-Q1 Example Code 0.1
). C:\ti\bq79616-Q1 Example Code 0.1
.