SLUUCG7 April 2024 BQ76922
If measurement of an interconnect between cells is not practical or desired, the BQ76922 device also includes fixed settings for cell interconnect resistance in Settings:Interconnect Resistances:Cell 1 Interconnect – Cell 5 Interconnect in units of mΩ. The device subtracts the measured current times these interconnect resistance values from each differential cell voltage measurement before reporting the final cell voltage value.