SLUUCK6A December 2021 – February 2022 TPSM8D6C24
Figure 10-2 shows the General Settings that can be used to configure the following:
After clicking Write to Hardware to make changes to one or more configurable parameters, the changes can be committed to nonvolatile memory by clicking Store Config to NVM. This action prompts a pop-up, and if confirmed, the changes are committed to nonvolatile memory to store all the modifications in nonvolatile memory.
Both the loop controller device and the loop follower device are tied to same bus interface. In a two-phase stacking system, the loop controller device will receive and respond to all PMBus communication and loop follower devices do not need to be connected to the PMBus. If the controller receives commands which require updates to the PMBus registers of the follower, the controller will relay these commands to the followers. All commands on this tab are for PHASE = 0xFF.