SLUUCK6A December 2021 – February 2022 TPSM8D6C24
The TPSM8D6C24EVM-2V0 includes a 49.9-Ω series resistor in the feedback loop for VOUT. The resistor is accessible at the test points TP7, TP8, TP19, and TP20 for loop response analysis. These test points should be used during loop response measurements as the perturbation injecting points for the loop. See the description in Table 6-2.
Test Point | Node Name | Description | Comment |
---|---|---|---|
VOUT_A | |||
TP7 | CHA_VoutA | Input to feedback divider of VOUT_A | The amplitude of the perturbation at this node should be limited to less than 30 mV. |
TP8 | CHB_VoutA | Resulting output of VOUT_A | Bode can be measured by a network analyzer with a CH_B/CH_A configuratio.n |
VOUT_B | |||
TP19 | CHA_VoutB | Input to feedback divider of VOUT_B | The amplitude of the perturbation at this node should be limited to less than 30 mV. |
TP20 | CHB_VoutB | Resulting output of VOUT_B | Bode can be measured by a network analyzer with a CH_B/CH_A configuration. |
Measure the loop response with the following procedure: