The following list of equipment is
recommended when testing with a constant voltage electronic load.
- Power Supplies:
A power supply capable of supplying 40 V at 8 A
is required. This part can handle larger voltage and current, however, larger
power levels are not necessary for this procedure. - Load 1:
Kikusui PLZ164WA 0-150 V, 0-33 A when testing without a real battery, connect
2000 uF of capacitance across the input. - Meters:
Six
Fluke 75 multimeters (equivalent or better) or three equivalent voltage meters
and three equivalent current meters. - Computer:
A
computer with at least one USB port and a USB cable. - EV2400 Communication Kit
- Software:
Download and properly install bqStudio.