SLUUD32A June 2024 – April 2025
The Registers section allows the user to view the reported parameters from the gauge. The Bit Registers section provides bit level picture of status and fault registers. A green background color indicates that the bit is 0 (low state) and a red background color indicates that the bit is 1 (high state). Data begins to update once the Refresh (single-time scan) button is selected, or scans continuously if the Scan button is selected.
Figure 4-1 Registers ScreenThe continuous scanning period can be set via the | Window | Preferences | SBS | Scan Interval | menu selections.
Battery Management Studio has the ability to record specific parameters over a period of time, which can be initiated by clicking the "Start Log" button. To specify which values to be recorded within the .log file, parameters can be selected using the Log check boxes located beside each parameter in the Register section. Logging can be stopped by pressing the "Stop Log" button.