SLUUD52 August 2024
Open the PMBus GUI shortcut on the desktop directly as shown in the following figure.
Figure 3-1 PMBus® GUIAfter opening the PMBus GUI , the specific PMBus address of TPS544E27 system view is shown in Figure 3-2. By default, the position of the shunt on the EVM jumper sets the TPS544E27 address to 0x7Bh. Click on Click to configure device.
Figure 3-2 PMBus® GUI System View