SLUUDH3 December 2025 AM62L
Follow the AM62L EVM Quick Start Guide to flash an SD Card and boot Linux on the TMDS62LEVM.
Connect the TMDS62LEVM's XDS110 port, which is next to the UART port, to the PC running the AM62L Power Visualizer using a microUSB cable. Refer to the Hardware section of the AM62L EVM User Guide.
Once the AM62L Power Visualizer is open, the user will need to install the TI Cloud Agent Application if its the first time in use. The TI Cloud Agent will allow for seemless connection and proper function of the XDS110 on-board debugger. Follow the instructions in the pop-up window to install the TI Cloud Agent.
Figure 1-1 TI Cloud Agent Installation. The AM62L Power Visualizer utilizes the XDS110 Firmware and its COM port to collect power data from the SoC and displays it. Go to Options > Serial Port Settings to set the correct COM port, its usually second COM port for the XDS110. Confirm the hardware connection at the bottom of the tool.
The tool itself will have the most up-to-date getting started instructions.