SLVAEG1A August 2019 – May 2021 TLV62568 , TLV62568A , TPS62840
In order to compare the three architectures, the tests conducted on each are as follows:
The setup for testing, shown in Figure 4-1, consists of:
Figure 4-1 Test Setup DiagramIn order to test and demonstrate these architectures, a test board with all three architectures was designed and fabricated. The board is shown in Figure 4-2, including the dimensions of each architecture on the board for form factor comparison. Note that all components on the board shown are on the top side of the board for direct comparison – the board area can be reduced by placement of components on both sides of the board.
Some ripple measurements taken were at or beneath the noise floor of the oscilloscope used, which was observed to be -86 dB (or 142 µVpp). These results are denoted as "Noise Floor" in the results table.
Figure 4-2 Test Board Image