SLVAFG6A December 2022 – November 2023 TPS25762-Q1 , TPS25772-Q1
This section includes example scenarios of port power allocation and distribution when using the different Multi-Port Power Allocation Policy and Power Distribution Rule options. The examples of when one or two Sinks are connected are shown in table format followed by a flow diagram. The tables concisely summarize what occurs when Sink devices connect to TPS25772-Q1 Source ports: the power requested by the Sinks and the power distributed to the Sinks. The flow diagrams that follow illustrate the PD negotiation between the Source and Sink using the same example scenarios.
A negotiation between Port Partners must successfully complete to establish a PD power contract. Port Partners communicate over the USB Type-C connector's CC wire and the typical PD negotiation process between a Sink and Source is outlined below: