Thermal design current (TDC) or
continuous maximum steady-state current,
Maximum amplitude (IMAX) of the
transient peak pulse current,
Maximum duration of the transient
peak pulse current,
Set the scalable fast-trip threshold
(ISFT) at around 1.2 times IMAX to allow the transient load current to
flow,
The over-current threshold (IOCP) is a
fraction of ISFT as depicted in Equation 6.
Equation 6.
By default, the value of k is 0.5 in TPS25984, TPS25985,
TPS25990, and TPS1685 eFuses. However, it is user-programmable in TPS25990 and TPS1685
eFuses through PMBus and pin strapping respectively. Afterword, the value of
RIMON resistance is obtained using Equation 4 and considering the actual value of k.
The fault timer duration needs to be set at more
than the maximum duration of the transient load current pulse whose amplitude is greater
than IOCP. The maximum possible fault timer duration is around 30ms. The fault
timer duration is PMBus programmable in TPS25990 and hardware programmable in the other
three eFuses by placing a ceramic capacitor on the ITIMER pin. The value of the capacitor
is obtained using Equation 5.
The number of eFuses in parallel needs to be
calculated based on the RMS current rating of the device and the RMS value of the total
system current or the TDC rating.