Here are five rubber stamp answers
which can give some insight on why this type of input network is needed:
- The 3-6db input network is there because on any general evaluation platform,
EVM, for any ADC manufacturer, the applications group has to design an EVM
attempting to cover the full analog bandwidth (BW) range that the ADC is capable
of covering. Also, there are all sorts of customers and end users with widely
varying applications so this input network approach is generic enough to handle
95% of what a customer can apply, analog signal-wise, into the ADC’s analog
inputs. If needed, the customer can later, decrease BW, make changes, or modify
the input network to design to their specific end application.
- The 3-6dB input network is
necessary for applications requiring the widest attainable BW of the ADC. Some
customers and applications need the full BW capability of the ADC. The resistive
network provides a good generic network that satisfies both the balun and ADC
impedance requirements. See Figure 2-1.
- The 3-6db input network is needed
for wider band balun in general. This type of network provides a stiff
impedance over a wide range of frequencies. Keep in mind the balun was
characterized with a VNA, which is a calibrated 50Ω environment over any
frequency range. When measuring the balun, the VNA provides a reference plane
that is more or less right at the point of each of the baluns primary inputs or
secondary outputs. So naturally if the balun was characterized this way, the
balun can want to see the characterized impedance close to the inputs or
outputs to resolve the baluns natural characterized frequency capability. Go
ahead, remove those three resistors on either side of the differential and let's
review the difference.
- Figure 2-2 shows exactly what can happen if you replace the attenuation network with a
straight, pass-through connection. See how the BW rolls off much faster without
that lossy or matching pad if we just use two pass-through interconnections
between the balun outputs and ADC’s analog inputs.
- The 3-6db input network is needed
because the ADC’s input impedance is not exact and even if the data sheet says
this is 100Ω differential, unfortunately it is not. See Figure 2-3, here is a measurement example of an SDD11 s-parameter smith chart of the
ADC12DJ5200RF analog inputs. Does that look like 100Ω differential across all
frequencies to you? I agree, this does not. It seems that lately, an increasing
number of designers consider the data sheet impedance specifications as literal
(and fixed) values, when in reality these only act as reference under specific
conditions. So please be mindful, and plop down a real termination resistor on
your PCB at, or near, any input or output to resolve a better impedance match
across a wide range of RF frequencies. Oh, and did I mention that most all IC
process nodes have variation on the order of ±20% for any or all specified
resistive terminations?
- The last reason the 3-6db input
network is needed, as frequency bandwidths go up and up, we are at 10GHz now,
next week this is 20GHz and so on. This drives the need for a wideband match as
indicated in the above points. However, placing a stiff impedance lossy pad also
helps to resolve any mismatch in impedance required by both the outputs of the
balun and inputs of the ADC. As you know, any mismatches in impedance starts to
create standing waves, which in turn causes ripples in the passband or band of
interest. By placing the lossy pad in between the balun outputs and ADC’s
inputs, this helps to resolve this mismatch and ultimately kills those
standing waves quickly without disrupting with AC performance, for example, SFDR
or spurious free dynamic range. Notice in Figure 2-4 how the ripples and reflections disappear quickly above 1GHz whenever the
3-6db pad is implemented.