SLVK226 October   2025 TPS7H4012-SEP

 

  1.   1
  2.   TPS7H4012-SEP and TPS7H4013-SEP Single-Event Effects (SEE)
  3.   Trademarks
  4. Introduction
  5. Single-Event Effects (SEE)
  6. Device and Test Board Information
  7. Irradiation Facility and Setup
  8. LETEFF and Range Calculation
  9. Test Setup and Procedures
  10. Destructive Single-Event Effects (DSEE)
    1. 7.1 Single-Event Latch-up (SEL) Results
    2. 7.2 Single-Event Burnout (SEB) and Single-Event Gate Rupture (SEGR) Results
  11. Single-Event Transients (SET)
  12. Event Rate Calculations
  13. 10Summary
  14.   A References

Single-Event Burnout (SEB) and Single-Event Gate Rupture (SEGR) Results

During the SEB/SEGR characterization, the device was tested at room temperature of ≈25°C. The device was tested under both the enabled and disabled mode. For the SEB-OFF mode the device was disabled using the EN-pin by forcing 0V (using Channel 1 of a E36311A Keysight PS). During the SEB/SEGR testing with the device enabled/disabled, not a single input current event was observed.

The species used for the SEB testing was 109Ag (TAMU) at 15 MeV/nucleon and 109Ag (KSEE) at 19.5 MeV/nucleon. For both ions an angle of incidence of 0° was used to achieve a LETEFF of ≈ 48 MeV×cm2/mg (for more details refer to Table 5-1). The kinetic energy in the vacuum for 109Ag (TAMU) is 1.635 GeV and 109Ag (KSEE) is 2.125 GeV. Flux of ≈105 ions/cm2/s and a fluence of ≈107 ions/cm2 per run was used. Run duration to achieve this fluence was ≈2 minutes. The seven devices (same as used in SEL testing) were powered up and exposed to the heavy-ions using the maximum recommended input voltage of 14V with the max recommended load for each respective device. No SEB/SEGR current events were observed during the 14 runs, indicating that the TPS7H401x-SEP is SEB/SEGR-free up to LETEFF = 48 MeV×cm2/mg and across the full electrical specifications. Table 8-4 shows the SEB/SEGR test conditions and results.

Table 7-2 Summary of TPS7H401x-SEP SEB/SEGR Test Condition and Results

Device

Run NumberUnit Number

Facility

IonLETEFF (MeV × cm2/mg)Flux (ions/cm2/s)Fluence (ions/cm2)Enabled StatusVIN (V)IOUT (A)SEB EVENT?

TPS7H4012-SEP

81

TAMU

109Ag

48

1.21 x 1059.99 x 106EN14

6

No
9TAMU109Ag481.00 × 1059.99 × 106DIS14

-

No
102TAMU109Ag481.03 × 1051.00 × 107EN14

6

No

11

TAMU109Ag489.97 × 1041.00 × 107DIS14-No

TPS7H4013-SEP

123TAMU109Ag481.13 × 1051.00 × 107EN143No
13TAMU109Ag481.27 × 1051.00 × 107DIS14-No
144TAMU109Ag481.25 × 1051.00 × 107EN14

3

No
15TAMU109Ag481.31 x 1051.00 x 107DIS14-No

TPS7H4012-SEP

16

5

KSEE

109Ag481.04 x 1051.00 x 107EN14

6

No

17

KSEE109Ag481.11 x 1051.00 x 107DIS14-No

18

6

KSEE109Ag481.07 x 1051.00 x 107EN14

6

No

19

KSEE109Ag481.06 x 1051.00 x 107DIS14-No

TPS7H4013-SEP

20

7

KSEE109Ag481.03 x 1051.00 x 107EN14

3

No

21

KSEE109Ag488.98 x 1041.00 x 107DIS14-No

Using the MFTF method described in Single-Event Effects (SEE) Confidence Interval Calculations application report, the upper-bound cross-section (using a 95% confidence level) is calculated as:

σSEB ≤ 2.63 × 10-8 cm2/device for LETEFF = 48 MeV×cm2/mg and T = 25°C.

 SEB On Current vs Time for Run 8 of the TPS7H4012-SEP at T = 25°C (VOUT = 3.3V)Figure 7-2 SEB On Current vs Time for Run 8 of the TPS7H4012-SEP at T = 25°C (VOUT = 3.3V)
 SEB Off Current vs Time for Run 9 of the TPS7H4012-SEP at T = 25°C (VOUT = 0V)Figure 7-3 SEB Off Current vs Time for Run 9 of the TPS7H4012-SEP at T = 25°C (VOUT = 0V)