SLVUCD1A May 2022 – September 2024
The README text box helps users connect the EVM board to the computer. If users want to see the README again, then users can access the README from the Help tab in the top left of the GUI dashboard. Here, users can also find an About option for information about the GUI version and additional documentation.
After users have dismissed the README message box, the GUI displays the Home page, shown in Figure 6-6. Here, users can see an overview of the TPS65219 power structure. The branching sections show what the alternate versions of the TPS65xxx family have to offer for a design.
At the bottom of the Home page, users can navigate to the other GUI pages, which are described in the subsequent sections. These pages can also be found on the left side of the GUI interface.
Figure 6-6 GUI Home Page