SLVUCP8A September   2024  – June 2025

 

  1.   1
  2.   Description
  3.   Get Started
  4.   Features
  5.   Applications
  6.   6
  7. 1Evaluation Module Overview
    1. 1.1 Introduction
    2. 1.2 Kit Contents
    3. 1.3 Specification
    4. 1.4 Device Information
  8. 2Hardware
    1. 2.1 Power Requirements
    2. 2.2 Setup
      1. 2.2.1 Flashing Firmware Configuration to the TPS26750EVM
      2. 2.2.2 Stand Alone Testing
      3. 2.2.3 Dead Battery Safe Mode
      4. 2.2.4 Dead Battery Always Enable Sink
      5. 2.2.5 TPS26750 and BQ25756
    3. 2.3 Header Information
    4. 2.4 Jumper Information
    5. 2.5 Push Buttons
    6. 2.6 Interfaces
    7. 2.7 Debug Information
    8. 2.8 Test Points and LEDS
  9. 3Software
    1. 3.1 Software Description
    2. 3.2 Software Installation
      1. 3.2.1 Web Browser
      2. 3.2.2 Native Application
    3. 3.3 Software Development
    4. 3.4 Using the Application Customization Tool
      1. 3.4.1 Default View
      2. 3.4.2 Selecting a Configuration
      3. 3.4.3 Filling Out the Questionnaire
      4. 3.4.4 Advanced Configuration Mode
      5. 3.4.5 Flashing Configuration to TPS26750
      6. 3.4.6 Additional Settings
        1. 3.4.6.1 Generating a New Configuration
        2. 3.4.6.2 Exporting and Importing Settings
        3. 3.4.6.3 Generating the Binary
        4. 3.4.6.4 Generating the VIF File
  10. 4Application Specific Use Cases
    1. 4.1 Use With the BQ25756EVM
      1. 4.1.1 Hardware Setup with BQ25756EVM
      2. 4.1.2 Software Setup with the BQ25756EVM
  11. 5Hardware Design Files
    1. 5.1 Schematics
    2. 5.2 PCB Layouts
    3. 5.3 Bill of Materials (BOM)
  12. 6Additional Information
    1. 6.1 Trademarks
    2. 6.2 Electrostatic Discharge Caution
    3. 6.3 Terminology
    4. 6.4 Device Support
      1. 6.4.1 Third-Party Products Disclaimer
      2. 6.4.2 Supplemental Content
    5. 6.5 Documentation Support
    6. 6.6 Receiving Notification of Documentation Updates
    7. 6.7 Support Resources
  13. 7Revision History

TPS26750 and BQ25756

TPS26750EVM TPS26750 and BQ25756 Block DiagramFigure 2-7 TPS26750 and BQ25756 Block Diagram

If users want to support 5V sourcing, then the power supply needs to provide at least 18W of power, due to the following board requirements:

  1. 5V 3A for PP5V Power Path
  2. 120mA for VCONN
  3. 100mA for Board MCU (U22)

If users want to support EPR sourcing (from 5V to 48V), then the power supply needs to provide at least 15V to the HV_SYS net (using either J3, J8. A battery can be connected to J8 for testing as well). However, the exact amount of power users need to provide depends on the expected load drawn by the sink and the highest voltage EPR contract users want to source.

The example setup in Figure 2-8 shows a 140W 3 Port PD3.1 Supported Wall Adapter, whose USB-C2 port is capable of providing 100W (20V at 5A) of power, connected to a USB-C to USB-C 100W capable cable, which is in turn connected to the Power Type C port (J3) of the TPS26750EVM. This example setup is capable of sourcing 48V of power to the DUT Type C port (J4), which is in the USB-PD Extended Power Range.

To source and sink power in the EPR range using the TPS26750EVM, users want connect a simulated battery to the HV_SYS header (J8) instead of powering the board through J3.


TPS26750EVM TPS26750EVM and BQ25756EVM Example Hardware Setup

Figure 2-8 TPS26750EVM and BQ25756EVM Example Hardware Setup
Note:

This figure depicts a previous version of the TPS26750 EVM (RevA2), but the information remains accurate and applicable to the current version.