SNAU297 July 2025
The Input page provides a high-level view of all the inputs for the device, the APLL frequencies, and DPLL frequencies of the device.
When the DPLL dividers and loop filter are calculated by running the script in step 8 on the start page, this page displays the DPLL divider values which set the DPLL frequency. This is shown that the DPLL frequency is the exact desired frequency.
The DPLL supports two sets of DPLL dividers, which can be selected. At this time, the tool calculates the divider for FB Config 1 only. To use two different feedback dividers, the following procedure must be preformed:
When using both feedback dividers, a requirement is not that the TDC rates are exactly the same; only that the TDC rates are within ±5% for the two DPLL feedback configurations.
Figure 3-12 APLL or DPLL Frequency
Selection