SNAU319 August   2025 LMK3H2108

 

  1.   1
  2.   Read This First
    1.     About This Manual
    2.     Notational Conventions
    3.     Glossary
    4.     Related Documentation
    5.     Support Resources
    6.     Trademarks
  3. 1Configuration Overview
    1. 1.1 LMK3H2108 Configuration Information
  4. 2Device Register Map
  5. 3Device Registers
  6. 4Revision History

Notational Conventions

This document uses the following conventions.

  • Hexadecimal numbers can be shown with the suffix h or the prefix 0x. For example, the following number is 40 hexadecimal (decimal 64): 40h or 0x40.
  • Registers in this document are shown in figures and described in tables.
    • Each register figure shows a rectangle divided into fields that represent the fields of the register. Each field is labeled with its bit name, its beginning and ending bit numbers above, and its read/write properties with default reset value below. A legend explains the notation used for the properties.
    • Reserved bits in a register figure can have one of multiple meanings:
      • Not implemented on the device
      • Reserved for future device expansion
      • Reserved for TI testing
      • Reserved configurations of the device that are not supported
    • Writing nondefault values to the Reserved bits could cause unexpected behavior and should be avoided.