SNVAA17 April   2021 LM25180-Q1 , LM25183-Q1 , LM25184-Q1 , LM5180 , LM5180-Q1 , LM5181-Q1

 

  1.   Trademarks
  2. 1Detailed Descriptions
    1. 1.1 Test Schematic
    2. 1.2 PCB Layout
  3. 2CISPR 25 Class 5 Conducted Emissions Results
  4. 3References

Test Schematic

The modified schematic shown in Figure 1-1, was used for all of the testing in this document. Modified components are shown in the red circles and in Table 1-1. The details of T1 and C3a are shown in Figure 1-2 and Figure 1-3. For more information, see the LM5180-Q1 Single-Output EVM User's Guide.

GUID-20210309-CA0I-ZKQF-DSKR-NBWDGTLKSVCQ-low.svg Figure 1-1 Modified EVM Schematic
Table 1-1 Changes to EVM
Reference Modification
C3a Added C3a; same value and location as C3; 0.1 μF
L2 Changed from 10 μH, Würth, 744042100 to 4.7 μH Würth, 744042004
C8, C10 Changed value of both capacitors from 22 pF to 100 pF
T1 Wrap transformer with copper shielding tape. Shield grounded at one point on primary side.
C1 Install C1. 1000 pF, 2kV, 1206, X7R
GUID-20210309-CA0I-HPLG-GCG9-TZQ7HB6XQLJ6-low.svgFigure 1-2 Copper Shielding of T1
GUID-20210309-CA0I-TGNB-BGT7-Z14C2RN6JMZW-low.svgFigure 1-3 Location of C3a