The following type of output file is created by the compiler:
- ELF object files. Executable and Linking Format (ELF) enables supporting modern language features like early template instantiation and exporting inline functions. ELF is part of the System V Application Binary Interface (ABI). The ELF format used for C6000 is extended by the C6000 Embedded Application Binary Interface (EABI), which is documented in SPRAB89.
COFF object files are not supported in v8.0 and later versions of the TI Code Generation Tools. If you would like to produce COFF output files, please use v7.4 of the Code Generation Tools and refer to SPRU186 for documentation.