SPRUIX1B October 2022 – April 2024 TMS320F2800132 , TMS320F2800133 , TMS320F2800135 , TMS320F2800137
Table 3-45 lists the memory-mapped registers for the CPU_SYS_REGS registers. All register offset addresses not listed in Table 3-45 should be considered as reserved locations and the register contents should not be modified.
| Offset | Acronym | Register Name | Write Protection | Section |
|---|---|---|---|---|
| 0h | CPUSYSLOCK1 | Lock bit for CPUSYS registers | EALLOW | Go |
| 2h | CPUSYSLOCK2 | Lock bit for CPUSYS registers | EALLOW | Go |
| Ah | PIEVERRADDR | PIE Vector Fetch Error Address register | EALLOW | Go |
| 22h | PCLKCR0 | Peripheral Clock Gating Registers | EALLOW | Go |
| 26h | PCLKCR2 | Peripheral Clock Gating Register - ETPWM | EALLOW | Go |
| 28h | PCLKCR3 | Peripheral Clock Gating Register - ECAP | EALLOW | Go |
| 2Ah | PCLKCR4 | Peripheral Clock Gating Register - EQEP | EALLOW | Go |
| 30h | PCLKCR7 | Peripheral Clock Gating Register - SCI | EALLOW | Go |
| 32h | PCLKCR8 | Peripheral Clock Gating Register - SPI | EALLOW | Go |
| 34h | PCLKCR9 | Peripheral Clock Gating Register - I2C | EALLOW | Go |
| 36h | PCLKCR10 | Peripheral Clock Gating Register - CAN | EALLOW | Go |
| 3Ch | PCLKCR13 | Peripheral Clock Gating Register - ADC | EALLOW | Go |
| 3Eh | PCLKCR14 | Peripheral Clock Gating Register - CMPSS | EALLOW | Go |
| 4Ch | PCLKCR21 | Peripheral Clock Gating Register - DCC | EALLOW | Go |
| 58h | PCLKCR27 | Peripheral Clock Gating Register - EPG | EALLOW | Go |
| 70h | SIMRESET | Simulated Reset Register | Go | |
| 76h | LPMCR | LPM Control Register | EALLOW | Go |
| 78h | GPIOLPMSEL0 | GPIO LPM Wakeup select registers | EALLOW | Go |
| 7Ah | GPIOLPMSEL1 | GPIO LPM Wakeup select registers | EALLOW | Go |
| 7Ch | TMR2CLKCTL | Timer2 Clock Measurement functionality control register | EALLOW | Go |
| 7Eh | RESCCLR | Reset Cause Clear Register | Go | |
| 80h | RESC | Reset Cause register | Go | |
| A0h | USER_REG1_SYSRSn | Software Configurable registers reset by SYSRSn | Go | |
| A2h | USER_REG2_SYSRSn | Software Configurable registers reset by SYSRSn | Go | |
| A4h | USER_REG1_XRSn | Software Configurable registers reset by XRSn | Go | |
| A6h | USER_REG2_XRSn | Software Configurable registers reset by XRSn | Go | |
| A8h | USER_REG1_PORESETn | Software Configurable registers reset by PORESETn | Go | |
| AAh | USER_REG2_PORESETn | Software Configurable registers reset by PORESETn | Go | |
| ACh | USER_REG3_PORESETn | Software Configurable registers reset by PORESETn | Go | |
| AEh | USER_REG4_PORESETn | Software Configurable registers reset by PORESETn | Go |
Complex bit access types are encoded to fit into small table cells. Table 3-46 shows the codes that are used for access types in this section.
| Access Type | Code | Description |
|---|---|---|
| Read Type | ||
| R | R | Read |
| R-0 | R -0 | Read Returns 0s |
| Write Type | ||
| W | W | Write |
| W1C | W 1C | Write 1 to clear |
| W1S | W 1S | Write 1 to set |
| WSonce | W Sonce | Write Set once |
| Reset or Default Value | ||
| -n | Value after reset or the default value | |
| Register Array Variables | ||
| i,j,k,l,m,n | When these variables are used in a register name, an offset, or an address, they refer to the value of a register array where the register is part of a group of repeating registers. The register groups form a hierarchical structure and the array is represented with a formula. | |
| y | When this variable is used in a register name, an offset, or an address it refers to the value of a register array. | |
CPUSYSLOCK1 is shown in Figure 3-39 and described in Table 3-47.
Return to the Summary Table.
Lock bit for CPUSYS registers
Notes:
[1] Any bit in this register, once set can only be cleared through a CPU1.SYSRSn. Write of 0 to any bit of this register has no effect
[2] The locking mechanism applies to only writes. Reads to the registers which have LOCK protection are always allowed
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| RESERVED | RESERVED | PCLKCR22 | PCLKCR21 | PCLKCR20 | RESERVED | RESERVED | RESERVED |
| R/WSonce-0h | R/WSonce-0h | R/WSonce-0h | R/WSonce-0h | R/WSonce-0h | R/WSonce-0h | R/WSonce-0h | R/WSonce-0h |
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| GPIOLPMSEL1 | GPIOLPMSEL0 | LPMCR | RESERVED | RESERVED | RESERVED | PCLKCR14 | PCLKCR13 |
| R/WSonce-0h | R/WSonce-0h | R/WSonce-0h | R/WSonce-0h | R/WSonce-0h | R/WSonce-0h | R/WSonce-0h | R/WSonce-0h |
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | RESERVED | PCLKCR10 | PCLKCR9 | PCLKCR8 | PCLKCR7 | PCLKCR6 | RESERVED |
| R/WSonce-0h | R/WSonce-0h | R/WSonce-0h | R/WSonce-0h | R/WSonce-0h | R/WSonce-0h | R/WSonce-0h | R/WSonce-0h |
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| PCLKCR4 | PCLKCR3 | PCLKCR2 | RESERVED | PCLKCR0 | PIEVERRADDR | RESERVED | RESERVED |
| R/WSonce-0h | R/WSonce-0h | R/WSonce-0h | R/WSonce-0h | R/WSonce-0h | R/WSonce-0h | R/WSonce-0h | R/WSonce-0h |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31 | RESERVED | R/WSonce | 0h | Reserved |
| 30 | RESERVED | R/WSonce | 0h | Reserved |
| 29 | PCLKCR22 | R/WSonce | 0h | Lock bit for PCLKCR22 Register: 0: Respective register is not locked 1: Respective register is locked. Reset type: SYSRSn |
| 28 | PCLKCR21 | R/WSonce | 0h | Lock bit for PCLKCR21 Register: 0: Respective register is not locked 1: Respective register is locked. Reset type: SYSRSn |
| 27 | PCLKCR20 | R/WSonce | 0h | Lock bit for PCLKCR20 Register: 0: Respective register is not locked 1: Respective register is locked. Reset type: SYSRSn |
| 26 | RESERVED | R/WSonce | 0h | Reserved |
| 25 | RESERVED | R/WSonce | 0h | Reserved |
| 24 | RESERVED | R/WSonce | 0h | Reserved |
| 23 | GPIOLPMSEL1 | R/WSonce | 0h | Lock bit for GPIOLPMSEL1 Register: 0: Respective register is not locked 1: Respective register is locked. Reset type: SYSRSn |
| 22 | GPIOLPMSEL0 | R/WSonce | 0h | Lock bit for GPIOLPMSEL0 Register: 0: Respective register is not locked 1: Respective register is locked. Reset type: SYSRSn |
| 21 | LPMCR | R/WSonce | 0h | Lock bit for LPMCR Register: 0: Respective register is not locked 1: Respective register is locked. Reset type: SYSRSn |
| 20 | RESERVED | R/WSonce | 0h | Reserved |
| 19 | RESERVED | R/WSonce | 0h | Reserved |
| 18 | RESERVED | R/WSonce | 0h | Reserved |
| 17 | PCLKCR14 | R/WSonce | 0h | Lock bit for PCLKCR14 Register: 0: Respective register is not locked 1: Respective register is locked. Reset type: SYSRSn |
| 16 | PCLKCR13 | R/WSonce | 0h | Lock bit for PCLKCR13 Register: 0: Respective register is not locked 1: Respective register is locked. Reset type: SYSRSn |
| 15 | RESERVED | R/WSonce | 0h | Reserved |
| 14 | RESERVED | R/WSonce | 0h | Reserved |
| 13 | PCLKCR10 | R/WSonce | 0h | Lock bit for PCLKCR10 Register: 0: Respective register is not locked 1: Respective register is locked. Reset type: SYSRSn |
| 12 | PCLKCR9 | R/WSonce | 0h | Lock bit for PCLKCR9 Register: 0: Respective register is not locked 1: Respective register is locked. Reset type: SYSRSn |
| 11 | PCLKCR8 | R/WSonce | 0h | Lock bit for PCLKCR8 Register: 0: Respective register is not locked 1: Respective register is locked. Reset type: SYSRSn |
| 10 | PCLKCR7 | R/WSonce | 0h | Lock bit for PCLKCR7 Register: 0: Respective register is not locked 1: Respective register is locked. Reset type: SYSRSn |
| 9 | PCLKCR6 | R/WSonce | 0h | Lock bit for PCLKCR6 Register: 0: Respective register is not locked 1: Respective register is locked. Reset type: SYSRSn |
| 8 | RESERVED | R/WSonce | 0h | Reserved |
| 7 | PCLKCR4 | R/WSonce | 0h | Lock bit for PCLKCR4 Register: 0: Respective register is not locked 1: Respective register is locked. Reset type: SYSRSn |
| 6 | PCLKCR3 | R/WSonce | 0h | Lock bit for PCLKCR3 Register: 0: Respective register is not locked 1: Respective register is locked. Reset type: SYSRSn |
| 5 | PCLKCR2 | R/WSonce | 0h | Lock bit for PCLKCR2 Register: 0: Respective register is not locked 1: Respective register is locked. Reset type: SYSRSn |
| 4 | RESERVED | R/WSonce | 0h | Reserved |
| 3 | PCLKCR0 | R/WSonce | 0h | Lock bit for PCLKCR0 Register: 0: Respective register is not locked 1: Respective register is locked. Reset type: SYSRSn |
| 2 | PIEVERRADDR | R/WSonce | 0h | Lock bit for PIEVERRADDR Register: 0: Respective register is not locked 1: Respective register is locked. Reset type: SYSRSn |
| 1 | RESERVED | R/WSonce | 0h | Reserved |
| 0 | RESERVED | R/WSonce | 0h | Reserved |
CPUSYSLOCK2 is shown in Figure 3-40 and described in Table 3-48.
Return to the Summary Table.
Lock bit for CPUSYS registers
Notes:
[1] Any bit in this register, once set can only be cleared through a CPU1.SYSRSn. Write of 0 to any bit of this register has no effect
[2] The locking mechanism applies to only writes. Reads to the registers which have LOCK protection are always allowed
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| USER_REG4_PORESETn | USER_REG3_PORESETn | USER_REG2_PORESETn | USER_REG1_PORESETn | USER_REG2_XRSn | USER_REG1_XRSn | USER_REG2_SYSRSn | USER_REG1_SYSRSn |
| R/WSonce-0h | R/WSonce-0h | R/WSonce-0h | R/WSonce-0h | R/WSonce-0h | R/WSonce-0h | R/WSonce-0h | R/WSonce-0h |
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | RESERVED | ||||||
| R/WSonce-0h | R-0-0h | ||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | |||||||
| R-0-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | RESERVED | PCLKCR27 | RESERVED | RESERVED | RESERVED | ||
| R-0-0h | R/WSonce-0h | R/WSonce-0h | R/WSonce-0h | R/WSonce-0h | R/WSonce-0h | ||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31 | USER_REG4_PORESETn | R/WSonce | 0h | Lock bit for USER_REG4_PORESETn Register 0: Respective register is not locked 1: Respective register is locked. Reset type: SYSRSn |
| 30 | USER_REG3_PORESETn | R/WSonce | 0h | Lock bit for USER_REG3_PORESETn Register 0: Respective register is not locked 1: Respective register is locked. Reset type: SYSRSn |
| 29 | USER_REG2_PORESETn | R/WSonce | 0h | Lock bit for USER_REG2_PORESETn Register 0: Respective register is not locked 1: Respective register is locked. Reset type: SYSRSn |
| 28 | USER_REG1_PORESETn | R/WSonce | 0h | Lock bit for USER_REG1_PORESETn Register 0: Respective register is not locked 1: Respective register is locked. Reset type: SYSRSn |
| 27 | USER_REG2_XRSn | R/WSonce | 0h | Lock bit for USER_REG2_XRSn Register 0: Respective register is not locked 1: Respective register is locked. Reset type: SYSRSn |
| 26 | USER_REG1_XRSn | R/WSonce | 0h | Lock bit for USER_REG1_XRSn Register 0: Respective register is not locked 1: Respective register is locked. Reset type: SYSRSn |
| 25 | USER_REG2_SYSRSn | R/WSonce | 0h | Lock bit for USER_REG2_SYSRSn Register 0: Respective register is not locked 1: Respective register is locked. Reset type: SYSRSn |
| 24 | USER_REG1_SYSRSn | R/WSonce | 0h | Lock bit for USER_REG1_SYSRSn Register 0: Respective register is not locked 1: Respective register is locked. Reset type: SYSRSn |
| 23 | RESERVED | R/WSonce | 0h | Reserved |
| 22-5 | RESERVED | R-0 | 0h | Reserved |
| 4 | RESERVED | R/WSonce | 0h | Reserved |
| 3 | PCLKCR27 | R/WSonce | 0h | Lock bit for PCLKCR27 Register: 0: Respective register is not locked 1: Respective register is locked. Reset type: SYSRSn |
| 2 | RESERVED | R/WSonce | 0h | Reserved |
| 1 | RESERVED | R/WSonce | 0h | Reserved |
| 0 | RESERVED | R/WSonce | 0h | Reserved |
PIEVERRADDR is shown in Figure 3-41 and described in Table 3-49.
Return to the Summary Table.
PIE Vector Fetch Error Address register
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | ADDR | ||||||||||||||||||||||||||||||
| R-0-0h | R/W-003FFFFFh | ||||||||||||||||||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-22 | RESERVED | R-0 | 0h | Reserved |
| 21-0 | ADDR | R/W | 003FFFFFh | This register defines the address of the PIE Vector Fetch Error handler routine. Its the responsibility of user to initialize this register. If this register is not initialized, a default error handler at address 0x3fffbe will get executed. Refer to the Boot ROM section for more details on this register. Reset type: XRSn |
PCLKCR0 is shown in Figure 3-42 and described in Table 3-50.
Return to the Summary Table.
Peripheral Clock Gating Registers
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| RESERVED | RESERVED | ||||||
| R-0-0h | R/W-0h | ||||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | RESERVED | TBCLKSYNC | RESERVED | HRCAL | |||
| R-0-0h | R/W-0h | R/W-0h | R-0-0h | R/W-0h | |||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | RESERVED | RESERVED | RESERVED | ||||
| R-0-0h | R/W-0h | R/W-0h | R-0-0h | ||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | CPUTIMER2 | CPUTIMER1 | CPUTIMER0 | RESERVED | RESERVED | RESERVED | |
| R-0-0h | R/W-1h | R/W-1h | R/W-1h | R/W-0h | R/W-0h | R/W-0h | |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-25 | RESERVED | R-0 | 0h | Reserved |
| 24 | RESERVED | R/W | 0h | Reserved |
| 23-20 | RESERVED | R-0 | 0h | Reserved |
| 19 | RESERVED | R/W | 0h | Reserved |
| 18 | TBCLKSYNC | R/W | 0h | EPWM Time Base Clock sync: When set PWM time bases of all the PWM modules belonging to the same CPU-Subsystem (as partitioned using their CPUSEL bits) start counting Reset type: SYSRSn |
| 17 | RESERVED | R-0 | 0h | Reserved |
| 16 | HRCAL | R/W | 0h | HRCAL Clock Enable Bit: When set, this enables the clock to the HRCAL module 1: HRCAL clock is enabled 0: HRCAL clock is disabled Reset type: SYSRSn |
| 15 | RESERVED | R-0 | 0h | Reserved |
| 14 | RESERVED | R/W | 0h | Reserved |
| 13 | RESERVED | R/W | 0h | Reserved |
| 12-6 | RESERVED | R-0 | 0h | Reserved |
| 5 | CPUTIMER2 | R/W | 1h | CPUTIMER2 Clock Enable bit: 0: Module clock is gated-off 1: Module clock is turned-on Reset type: SYSRSn |
| 4 | CPUTIMER1 | R/W | 1h | CPUTIMER1 Clock Enable bit: 0: Module clock is gated-off 1: Module clock is turned-on Reset type: SYSRSn |
| 3 | CPUTIMER0 | R/W | 1h | CPUTIMER0 Clock Enable bit: 0: Module clock is gated-off 1: Module clock is turned-on Reset type: SYSRSn |
| 2 | RESERVED | R/W | 0h | Reserved |
| 1 | RESERVED | R/W | 0h | Reserved |
| 0 | RESERVED | R/W | 0h | Reserved |
PCLKCR2 is shown in Figure 3-43 and described in Table 3-51.
Return to the Summary Table.
Peripheral Clock Gating Register - ETPWM
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| RESERVED | |||||||
| R-0-0h | |||||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | |||||||
| R-0-0h | |||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | RESERVED | RESERVED | RESERVED | RESERVED | RESERVED | RESERVED | RESERVED |
| R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h |
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | EPWM7 | EPWM6 | EPWM5 | EPWM4 | EPWM3 | EPWM2 | EPWM1 |
| R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-16 | RESERVED | R-0 | 0h | Reserved |
| 15 | RESERVED | R/W | 0h | Reserved |
| 14 | RESERVED | R/W | 0h | Reserved |
| 13 | RESERVED | R/W | 0h | Reserved |
| 12 | RESERVED | R/W | 0h | Reserved |
| 11 | RESERVED | R/W | 0h | Reserved |
| 10 | RESERVED | R/W | 0h | Reserved |
| 9 | RESERVED | R/W | 0h | Reserved |
| 8 | RESERVED | R/W | 0h | Reserved |
| 7 | RESERVED | R/W | 0h | Reserved |
| 6 | EPWM7 | R/W | 0h | EPWM7 Clock Enable bit: 0: Module clock is gated-off 1: Module clock is turned-on Reset type: SYSRSn |
| 5 | EPWM6 | R/W | 0h | EPWM6 Clock Enable bit: 0: Module clock is gated-off 1: Module clock is turned-on Reset type: SYSRSn |
| 4 | EPWM5 | R/W | 0h | EPWM5 Clock Enable bit: 0: Module clock is gated-off 1: Module clock is turned-on Reset type: SYSRSn |
| 3 | EPWM4 | R/W | 0h | EPWM4 Clock Enable bit: 0: Module clock is gated-off 1: Module clock is turned-on Reset type: SYSRSn |
| 2 | EPWM3 | R/W | 0h | EPWM3 Clock Enable bit: 0: Module clock is gated-off 1: Module clock is turned-on Reset type: SYSRSn |
| 1 | EPWM2 | R/W | 0h | EPWM2 Clock Enable bit: 0: Module clock is gated-off 1: Module clock is turned-on Reset type: SYSRSn |
| 0 | EPWM1 | R/W | 0h | EPWM1 Clock Enable bit: 0: Module clock is gated-off 1: Module clock is turned-on Reset type: SYSRSn |
PCLKCR3 is shown in Figure 3-44 and described in Table 3-52.
Return to the Summary Table.
Peripheral Clock Gating Register - ECAP
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| RESERVED | |||||||
| R-0-0h | |||||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | |||||||
| R-0-0h | |||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | |||||||
| R-0-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | RESERVED | RESERVED | RESERVED | RESERVED | RESERVED | ECAP2 | ECAP1 |
| R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-8 | RESERVED | R-0 | 0h | Reserved |
| 7 | RESERVED | R/W | 0h | Reserved |
| 6 | RESERVED | R/W | 0h | Reserved |
| 5 | RESERVED | R/W | 0h | Reserved |
| 4 | RESERVED | R/W | 0h | Reserved |
| 3 | RESERVED | R/W | 0h | Reserved |
| 2 | RESERVED | R/W | 0h | Reserved |
| 1 | ECAP2 | R/W | 0h | ECAP2 Clock Enable bit: 0: Module clock is gated-off 1: Module clock is turned-on Reset type: SYSRSn |
| 0 | ECAP1 | R/W | 0h | ECAP1 Clock Enable bit: 0: Module clock is gated-off 1: Module clock is turned-on Reset type: SYSRSn |
PCLKCR4 is shown in Figure 3-45 and described in Table 3-53.
Return to the Summary Table.
Peripheral Clock Gating Register - EQEP
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| RESERVED | |||||||
| R-0-0h | |||||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | |||||||
| R-0-0h | |||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | |||||||
| R-0-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | RESERVED | RESERVED | RESERVED | EQEP1 | |||
| R-0-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | |||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-4 | RESERVED | R-0 | 0h | Reserved |
| 3 | RESERVED | R/W | 0h | Reserved |
| 2 | RESERVED | R/W | 0h | Reserved |
| 1 | RESERVED | R/W | 0h | Reserved |
| 0 | EQEP1 | R/W | 0h | EQEP1 Clock Enable bit: 0: Module clock is gated-off 1: Module clock is turned-on Reset type: SYSRSn |
PCLKCR7 is shown in Figure 3-46 and described in Table 3-54.
Return to the Summary Table.
Peripheral Clock Gating Register - SCI
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| RESERVED | |||||||
| R-0-0h | |||||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | |||||||
| R-0-0h | |||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | |||||||
| R-0-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | RESERVED | SCI_C | SCI_B | SCI_A | |||
| R-0-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | |||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-4 | RESERVED | R-0 | 0h | Reserved |
| 3 | RESERVED | R/W | 0h | Reserved |
| 2 | SCI_C | R/W | 0h | SCI_C Clock Enable bit: 0: Module clock is gated-off 1: Module clock is turned-on Reset type: SYSRSn |
| 1 | SCI_B | R/W | 0h | SCI_B Clock Enable bit: 0: Module clock is gated-off 1: Module clock is turned-on Reset type: SYSRSn |
| 0 | SCI_A | R/W | 0h | SCI_A Clock Enable bit: 0: Module clock is gated-off 1: Module clock is turned-on Reset type: SYSRSn |
PCLKCR8 is shown in Figure 3-47 and described in Table 3-55.
Return to the Summary Table.
Peripheral Clock Gating Register - SPI
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| RESERVED | |||||||
| R-0-0h | |||||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | RESERVED | RESERVED | |||||
| R-0-0h | R/W-0h | R/W-0h | |||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | |||||||
| R-0-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | RESERVED | RESERVED | RESERVED | SPI_A | |||
| R-0-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | |||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-18 | RESERVED | R-0 | 0h | Reserved |
| 17 | RESERVED | R/W | 0h | Reserved |
| 16 | RESERVED | R/W | 0h | Reserved |
| 15-4 | RESERVED | R-0 | 0h | Reserved |
| 3 | RESERVED | R/W | 0h | Reserved |
| 2 | RESERVED | R/W | 0h | Reserved |
| 1 | RESERVED | R/W | 0h | Reserved |
| 0 | SPI_A | R/W | 0h | SPI_A Clock Enable bit: 0: Module clock is gated-off 1: Module clock is turned-on Reset type: SYSRSn |
PCLKCR9 is shown in Figure 3-48 and described in Table 3-56.
Return to the Summary Table.
Peripheral Clock Gating Register - I2C
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| RESERVED | |||||||
| R-0-0h | |||||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | |||||||
| R-0-0h | |||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | |||||||
| R-0-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | I2C_B | I2C_A | |||||
| R-0-0h | R/W-0h | R/W-0h | |||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-2 | RESERVED | R-0 | 0h | Reserved |
| 1 | I2C_B | R/W | 0h | I2C_B Clock Enable bit: 0: Module clock is gated-off 1: Module clock is turned-on Reset type: SYSRSn |
| 0 | I2C_A | R/W | 0h | I2C_A Clock Enable bit: 0: Module clock is gated-off 1: Module clock is turned-on Reset type: SYSRSn |
PCLKCR10 is shown in Figure 3-49 and described in Table 3-57.
Return to the Summary Table.
Peripheral Clock Gating Register - CAN
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| RESERVED | |||||||
| R-0-0h | |||||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | |||||||
| R-0-0h | |||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | |||||||
| R-0-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | RESERVED | RESERVED | RESERVED | RESERVED | RESERVED | RESERVED | CAN_A |
| R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-8 | RESERVED | R-0 | 0h | Reserved |
| 7 | RESERVED | R/W | 0h | Reserved |
| 6 | RESERVED | R/W | 0h | Reserved |
| 5 | RESERVED | R/W | 0h | Reserved |
| 4 | RESERVED | R/W | 0h | Reserved |
| 3 | RESERVED | R/W | 0h | Reserved |
| 2 | RESERVED | R/W | 0h | Reserved |
| 1 | RESERVED | R/W | 0h | Reserved |
| 0 | CAN_A | R/W | 0h | CAN_A Clock Enable bit: 0: Module clock is gated-off 1: Module clock is turned-on Reset type: SYSRSn |
PCLKCR13 is shown in Figure 3-50 and described in Table 3-58.
Return to the Summary Table.
Peripheral Clock Gating Register - ADC
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| RESERVED | |||||||
| R-0-0h | |||||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | |||||||
| R-0-0h | |||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | |||||||
| R-0-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | RESERVED | ADC_C | RESERVED | ADC_A | |||
| R-0-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | |||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-4 | RESERVED | R-0 | 0h | Reserved |
| 3 | RESERVED | R/W | 0h | Reserved |
| 2 | ADC_C | R/W | 0h | ADC_C Clock Enable bit: 0: Module clock is gated-off 1: Module clock is turned-on Reset type: SYSRSn |
| 1 | RESERVED | R/W | 0h | Reserved |
| 0 | ADC_A | R/W | 0h | ADC_A Clock Enable bit: 0: Module clock is gated-off 1: Module clock is turned-on Reset type: SYSRSn |
PCLKCR14 is shown in Figure 3-51 and described in Table 3-59.
Return to the Summary Table.
Peripheral Clock Gating Register - CMPSS
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| RESERVED | |||||||
| R-0-0h | |||||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | |||||||
| R-0-0h | |||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | |||||||
| R-0-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | RESERVED | RESERVED | RESERVED | CMPSS4 | CMPSS3 | CMPSS2 | CMPSS1 |
| R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-8 | RESERVED | R-0 | 0h | Reserved |
| 7 | RESERVED | R/W | 0h | Reserved |
| 6 | RESERVED | R/W | 0h | Reserved |
| 5 | RESERVED | R/W | 0h | Reserved |
| 4 | RESERVED | R/W | 0h | Reserved |
| 3 | CMPSS4 | R/W | 0h | CMPSS4 Clock Enable bit: 0: Module clock is gated-off 1: Module clock is turned-on Reset type: SYSRSn |
| 2 | CMPSS3 | R/W | 0h | CMPSS3 Clock Enable bit: 0: Module clock is gated-off 1: Module clock is turned-on Reset type: SYSRSn |
| 1 | CMPSS2 | R/W | 0h | CMPSS2 Clock Enable bit: 0: Module clock is gated-off 1: Module clock is turned-on Reset type: SYSRSn |
| 0 | CMPSS1 | R/W | 0h | CMPSS1 Clock Enable bit: 0: Module clock is gated-off 1: Module clock is turned-on Reset type: SYSRSn |
PCLKCR21 is shown in Figure 3-52 and described in Table 3-60.
Return to the Summary Table.
Peripheral Clock Gating Register - DCC
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| RESERVED | |||||||
| R-0-0h | |||||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | |||||||
| R-0-0h | |||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | |||||||
| R-0-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | RESERVED | DCC0 | |||||
| R-0-0h | R/W-0h | R/W-0h | |||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-2 | RESERVED | R-0 | 0h | Reserved |
| 1 | RESERVED | R/W | 0h | Reserved |
| 0 | DCC0 | R/W | 0h | DCC Clock Enable Bit: 0: Module clock is gated-off 1: Module clock is turned-on Reset type: SYSRSn |
PCLKCR27 is shown in Figure 3-53 and described in Table 3-61.
Return to the Summary Table.
Peripheral Clock Gating Register - EPG
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| RESERVED | |||||||
| R-0-0h | |||||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | |||||||
| R-0-0h | |||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | |||||||
| R-0-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | EPG1 | ||||||
| R-0-0h | R/W-0h | ||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-1 | RESERVED | R-0 | 0h | Reserved |
| 0 | EPG1 | R/W | 0h | EPG1 Clock Enable Bit: 0: Module clock is gated-off 1: Module clock is turned-on Reset type: SYSRSn |
SIMRESET is shown in Figure 3-54 and described in Table 3-62.
Return to the Summary Table.
Simulated Reset Register
Note: This register exists only on CPU1
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| KEY | |||||||
| R-0/W-0h | |||||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| KEY | |||||||
| R-0/W-0h | |||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | |||||||
| R-0-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | XRSn | CPU1RSn | |||||
| R-0-0h | R-0/W1S-0h | R-0/W1S-0h | |||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-16 | KEY | R-0/W | 0h | Write to this register succeeds only if this field is written with a value of 0xa5a5 Note: [1] Due to this KEY, only 32-bit writes will succeed (provided the KEY matches). 16-bit writes to the upper or lower half of this register will be ignored Reset type: XRSn |
| 15-2 | RESERVED | R-0 | 0h | Reserved |
| 1 | XRSn | R-0/W1S | 0h | Writing a 1 to this field generates a XRSn like reset. Writing a 0 has no effect. Note: Writing to this pin will pull the XRSn pin low for 512 INTOSC1 clock cycles. Reset type: XRSn |
| 0 | CPU1RSn | R-0/W1S | 0h | Writing a 1 to this field generates a reset to to CPU1. Writing a 0 has no effect. Reset type: XRSn |
LPMCR is shown in Figure 3-55 and described in Table 3-63.
Return to the Summary Table.
LPM Control Register
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| RESERVED | RESERVED | ||||||
| R/W1S-0h | R-0-0h | ||||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | RESERVED | ||||||
| R-0-0h | R/W-0h | ||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| WDINTE | RESERVED | ||||||
| R/W-0h | R-0-0h | ||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| QUALSTDBY | LPM | ||||||
| R/W-3Fh | R/W-0h | ||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31 | RESERVED | R/W1S | 0h | Reserved |
| 30-18 | RESERVED | R-0 | 0h | Reserved |
| 17-16 | RESERVED | R/W | 0h | Reserved |
| 15 | WDINTE | R/W | 0h | When this bit is set to 1, it enables the watchdog interrupt signal to wake the device from STANDBY mode. Note: [1] To use this signal, the user must also enable the WDINTn signal using the WDENINT bit in the SCSR register. This signal will not wake the device from HALT mode because the clock to watchdog module is turned off Reset type: SYSRSn |
| 14-8 | RESERVED | R-0 | 0h | Reserved |
| 7-2 | QUALSTDBY | R/W | 3Fh | Select number of OSCCLK clock cycles to qualify the selected inputs when waking the from STANDBY mode: 000000 = 2 OSCCLKs 000001 = 3 OSCCLKs ...... 111111 = 65 OSCCLKs Note: The LPMCR.QUALSTDBY register should be set to a value greater than the ratio of INTOSC1/PLLSYSCLK to ensure proper wake up. Reset type: SYSRSn |
| 1-0 | LPM | R/W | 0h | These bits set the low power mode for the device. Takes effect when CPU executes the IDLE instruction (when IDLE instruction is out of EXE Phase of the Pipeline) 00: IDLE Mode 01: STANDBY Mode 1x: HALT Mode Reset type: SYSRSn |
GPIOLPMSEL0 is shown in Figure 3-56 and described in Table 3-64.
Return to the Summary Table.
GPIO LPM Wakeup select registers
Connects the selected pin to the LPM circuit. Refer to LPM section of the TRM for the wakeup capabilities of the selected pin.
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| GPIO31 | GPIO30 | GPIO29 | GPIO28 | GPIO27 | GPIO26 | GPIO25 | GPIO24 |
| R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h |
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| GPIO23 | GPIO22 | GPIO21 | GPIO20 | GPIO19 | GPIO18 | GPIO17 | GPIO16 |
| R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h |
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| GPIO15 | GPIO14 | GPIO13 | GPIO12 | GPIO11 | GPIO10 | GPIO9 | GPIO8 |
| R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h |
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| GPIO7 | GPIO6 | GPIO5 | GPIO4 | GPIO3 | GPIO2 | GPIO1 | GPIO0 |
| R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31 | GPIO31 | R/W | 0h | 0 pin is dis-connected from LPM circuit 1 pin is connected to LPM circuit Reset type: SYSRSn |
| 30 | GPIO30 | R/W | 0h | 0 pin is dis-connected from LPM circuit 1 pin is connected to LPM circuit Reset type: SYSRSn |
| 29 | GPIO29 | R/W | 0h | 0 pin is dis-connected from LPM circuit 1 pin is connected to LPM circuit Reset type: SYSRSn |
| 28 | GPIO28 | R/W | 0h | 0 pin is dis-connected from LPM circuit 1 pin is connected to LPM circuit Reset type: SYSRSn |
| 27 | GPIO27 | R/W | 0h | 0 pin is dis-connected from LPM circuit 1 pin is connected to LPM circuit Reset type: SYSRSn |
| 26 | GPIO26 | R/W | 0h | 0 pin is dis-connected from LPM circuit 1 pin is connected to LPM circuit Reset type: SYSRSn |
| 25 | GPIO25 | R/W | 0h | 0 pin is dis-connected from LPM circuit 1 pin is connected to LPM circuit Reset type: SYSRSn |
| 24 | GPIO24 | R/W | 0h | 0 pin is dis-connected from LPM circuit 1 pin is connected to LPM circuit Reset type: SYSRSn |
| 23 | GPIO23 | R/W | 0h | 0 pin is dis-connected from LPM circuit 1 pin is connected to LPM circuit Reset type: SYSRSn |
| 22 | GPIO22 | R/W | 0h | 0 pin is dis-connected from LPM circuit 1 pin is connected to LPM circuit Reset type: SYSRSn |
| 21 | GPIO21 | R/W | 0h | 0 pin is dis-connected from LPM circuit 1 pin is connected to LPM circuit Reset type: SYSRSn |
| 20 | GPIO20 | R/W | 0h | 0 pin is dis-connected from LPM circuit 1 pin is connected to LPM circuit Reset type: SYSRSn |
| 19 | GPIO19 | R/W | 0h | 0 pin is dis-connected from LPM circuit 1 pin is connected to LPM circuit Reset type: SYSRSn |
| 18 | GPIO18 | R/W | 0h | 0 pin is dis-connected from LPM circuit 1 pin is connected to LPM circuit Reset type: SYSRSn |
| 17 | GPIO17 | R/W | 0h | 0 pin is dis-connected from LPM circuit 1 pin is connected to LPM circuit Reset type: SYSRSn |
| 16 | GPIO16 | R/W | 0h | 0 pin is dis-connected from LPM circuit 1 pin is connected to LPM circuit Reset type: SYSRSn |
| 15 | GPIO15 | R/W | 0h | 0 pin is dis-connected from LPM circuit 1 pin is connected to LPM circuit Reset type: SYSRSn |
| 14 | GPIO14 | R/W | 0h | 0 pin is dis-connected from LPM circuit 1 pin is connected to LPM circuit Reset type: SYSRSn |
| 13 | GPIO13 | R/W | 0h | 0 pin is dis-connected from LPM circuit 1 pin is connected to LPM circuit Reset type: SYSRSn |
| 12 | GPIO12 | R/W | 0h | 0 pin is dis-connected from LPM circuit 1 pin is connected to LPM circuit Reset type: SYSRSn |
| 11 | GPIO11 | R/W | 0h | 0 pin is dis-connected from LPM circuit 1 pin is connected to LPM circuit Reset type: SYSRSn |
| 10 | GPIO10 | R/W | 0h | 0 pin is dis-connected from LPM circuit 1 pin is connected to LPM circuit Reset type: SYSRSn |
| 9 | GPIO9 | R/W | 0h | 0 pin is dis-connected from LPM circuit 1 pin is connected to LPM circuit Reset type: SYSRSn |
| 8 | GPIO8 | R/W | 0h | 0 pin is dis-connected from LPM circuit 1 pin is connected to LPM circuit Reset type: SYSRSn |
| 7 | GPIO7 | R/W | 0h | 0 pin is dis-connected from LPM circuit 1 pin is connected to LPM circuit Reset type: SYSRSn |
| 6 | GPIO6 | R/W | 0h | 0 pin is dis-connected from LPM circuit 1 pin is connected to LPM circuit Reset type: SYSRSn |
| 5 | GPIO5 | R/W | 0h | 0 pin is dis-connected from LPM circuit 1 pin is connected to LPM circuit Reset type: SYSRSn |
| 4 | GPIO4 | R/W | 0h | 0 pin is dis-connected from LPM circuit 1 pin is connected to LPM circuit Reset type: SYSRSn |
| 3 | GPIO3 | R/W | 0h | 0 pin is dis-connected from LPM circuit 1 pin is connected to LPM circuit Reset type: SYSRSn |
| 2 | GPIO2 | R/W | 0h | 0 pin is dis-connected from LPM circuit 1 pin is connected to LPM circuit Reset type: SYSRSn |
| 1 | GPIO1 | R/W | 0h | 0 pin is dis-connected from LPM circuit 1 pin is connected to LPM circuit Reset type: SYSRSn |
| 0 | GPIO0 | R/W | 0h | 0 pin is dis-connected from LPM circuit 1 pin is connected to LPM circuit Reset type: SYSRSn |
GPIOLPMSEL1 is shown in Figure 3-57 and described in Table 3-65.
Return to the Summary Table.
GPIO LPM Wakeup select registers
Connects the selected pin to the LPM circuit. Refer to LPM section of the TRM for the wakeup capabilities of the selected pin.
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| GPIO63 | GPIO62 | GPIO61 | GPIO60 | GPIO59 | GPIO58 | GPIO57 | GPIO56 |
| R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h |
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| GPIO55 | GPIO54 | GPIO53 | GPIO52 | GPIO51 | GPIO50 | GPIO49 | GPIO48 |
| R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h |
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| GPIO47 | GPIO46 | GPIO45 | GPIO44 | GPIO43 | GPIO42 | GPIO41 | GPIO40 |
| R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h |
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| GPIO39 | GPIO38 | GPIO37 | GPIO36 | GPIO35 | GPIO34 | GPIO33 | GPIO32 |
| R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31 | GPIO63 | R/W | 0h | 0 pin is dis-connected from LPM circuit 1 pin is connected to LPM circuit Reset type: SYSRSn |
| 30 | GPIO62 | R/W | 0h | 0 pin is dis-connected from LPM circuit 1 pin is connected to LPM circuit Reset type: SYSRSn |
| 29 | GPIO61 | R/W | 0h | 0 pin is dis-connected from LPM circuit 1 pin is connected to LPM circuit Reset type: SYSRSn |
| 28 | GPIO60 | R/W | 0h | 0 pin is dis-connected from LPM circuit 1 pin is connected to LPM circuit Reset type: SYSRSn |
| 27 | GPIO59 | R/W | 0h | 0 pin is dis-connected from LPM circuit 1 pin is connected to LPM circuit Reset type: SYSRSn |
| 26 | GPIO58 | R/W | 0h | 0 pin is dis-connected from LPM circuit 1 pin is connected to LPM circuit Reset type: SYSRSn |
| 25 | GPIO57 | R/W | 0h | 0 pin is dis-connected from LPM circuit 1 pin is connected to LPM circuit Reset type: SYSRSn |
| 24 | GPIO56 | R/W | 0h | 0 pin is dis-connected from LPM circuit 1 pin is connected to LPM circuit Reset type: SYSRSn |
| 23 | GPIO55 | R/W | 0h | 0 pin is dis-connected from LPM circuit 1 pin is connected to LPM circuit Reset type: SYSRSn |
| 22 | GPIO54 | R/W | 0h | 0 pin is dis-connected from LPM circuit 1 pin is connected to LPM circuit Reset type: SYSRSn |
| 21 | GPIO53 | R/W | 0h | 0 pin is dis-connected from LPM circuit 1 pin is connected to LPM circuit Reset type: SYSRSn |
| 20 | GPIO52 | R/W | 0h | 0 pin is dis-connected from LPM circuit 1 pin is connected to LPM circuit Reset type: SYSRSn |
| 19 | GPIO51 | R/W | 0h | 0 pin is dis-connected from LPM circuit 1 pin is connected to LPM circuit Reset type: SYSRSn |
| 18 | GPIO50 | R/W | 0h | 0 pin is dis-connected from LPM circuit 1 pin is connected to LPM circuit Reset type: SYSRSn |
| 17 | GPIO49 | R/W | 0h | 0 pin is dis-connected from LPM circuit 1 pin is connected to LPM circuit Reset type: SYSRSn |
| 16 | GPIO48 | R/W | 0h | 0 pin is dis-connected from LPM circuit 1 pin is connected to LPM circuit Reset type: SYSRSn |
| 15 | GPIO47 | R/W | 0h | 0 pin is dis-connected from LPM circuit 1 pin is connected to LPM circuit Reset type: SYSRSn |
| 14 | GPIO46 | R/W | 0h | 0 pin is dis-connected from LPM circuit 1 pin is connected to LPM circuit Reset type: SYSRSn |
| 13 | GPIO45 | R/W | 0h | 0 pin is dis-connected from LPM circuit 1 pin is connected to LPM circuit Reset type: SYSRSn |
| 12 | GPIO44 | R/W | 0h | 0 pin is dis-connected from LPM circuit 1 pin is connected to LPM circuit Reset type: SYSRSn |
| 11 | GPIO43 | R/W | 0h | 0 pin is dis-connected from LPM circuit 1 pin is connected to LPM circuit Reset type: SYSRSn |
| 10 | GPIO42 | R/W | 0h | 0 pin is dis-connected from LPM circuit 1 pin is connected to LPM circuit Reset type: SYSRSn |
| 9 | GPIO41 | R/W | 0h | 0 pin is dis-connected from LPM circuit 1 pin is connected to LPM circuit Reset type: SYSRSn |
| 8 | GPIO40 | R/W | 0h | 0 pin is dis-connected from LPM circuit 1 pin is connected to LPM circuit Reset type: SYSRSn |
| 7 | GPIO39 | R/W | 0h | 0 pin is dis-connected from LPM circuit 1 pin is connected to LPM circuit Reset type: SYSRSn |
| 6 | GPIO38 | R/W | 0h | 0 pin is dis-connected from LPM circuit 1 pin is connected to LPM circuit Reset type: SYSRSn |
| 5 | GPIO37 | R/W | 0h | 0 pin is dis-connected from LPM circuit 1 pin is connected to LPM circuit Reset type: SYSRSn |
| 4 | GPIO36 | R/W | 0h | 0 pin is dis-connected from LPM circuit 1 pin is connected to LPM circuit Reset type: SYSRSn |
| 3 | GPIO35 | R/W | 0h | 0 pin is dis-connected from LPM circuit 1 pin is connected to LPM circuit Reset type: SYSRSn |
| 2 | GPIO34 | R/W | 0h | 0 pin is dis-connected from LPM circuit 1 pin is connected to LPM circuit Reset type: SYSRSn |
| 1 | GPIO33 | R/W | 0h | 0 pin is dis-connected from LPM circuit 1 pin is connected to LPM circuit Reset type: SYSRSn |
| 0 | GPIO32 | R/W | 0h | 0 pin is dis-connected from LPM circuit 1 pin is connected to LPM circuit Reset type: SYSRSn |
TMR2CLKCTL is shown in Figure 3-58 and described in Table 3-66.
Return to the Summary Table.
Timer2 Clock Measurement functionality control register
This memory mapped register requires a delay of 45 SYSCLK cycles between subsequent writes to the register, otherwise a second write can be lost. This delay can be realized by adding 45 NOP instructions.
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| RESERVED | |||||||
| R-0-0h | |||||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | |||||||
| R-0-0h | |||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | |||||||
| R-0-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | TMR2CLKPRESCALE | TMR2CLKSRCSEL | |||||
| R-0-0h | R/W-0h | R/W-0h | |||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-6 | RESERVED | R-0 | 0h | Reserved |
| 5-3 | TMR2CLKPRESCALE | R/W | 0h | CPU Timer 2 Clock Pre-Scale Value: These bits select the pre-scale value for the selected clock source for CPU Timer 2: 0,0,0,/1 (default on reset) 0,0,1,/2, 0,1,0,/4 0,1,1,/8 1,0,0,/16 1,0,1,spare (defaults to /16) 1,1,0,spare (defaults to /16) 1,1,1,spare (defaults to /16) Note: [1] The CPU Timer2s Clock sync logic detects an input clock edge when configured for any clock source other than SYSCLK and generates an appropriate clock pulse to the CPU timer2. If SYSCLK is approximately the same or less then the input clock source, then the user would need to configure the pre-scale value such that SYSCLK is at least twice as fast as the pre-scaled value. Reset type: SYSRSn |
| 2-0 | TMR2CLKSRCSEL | R/W | 0h | CPU Timer 2 Clock Source Select Bit: This bit selects the source for CPU Timer 2: 000 =SYSCLK Selected (default on reset, pre-scale is bypassed) 001 = INTOSC1 010 = INTOSC2 011 = XTAL 100 = PUMPOSC (from no-wrapper) 101 = FOSCCLK (Reserved) 110 = AUXPLLCLK (Reserved) 111 = reserved Reset type: SYSRSn |
RESCCLR is shown in Figure 3-59 and described in Table 3-67.
Return to the Summary Table.
Reset Cause Clear Register
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| RESERVED | |||||||
| R-0-0h | |||||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | |||||||
| R-0-0h | |||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | SIMRESET_XRSn | SIMRESET_CPU1RSn | RESERVED | SCCRESETn | |||
| R-0-0h | W1C-0h | W1C-0h | R-0-0h | W1S-0h | |||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | RESERVED | RESERVED | RESERVED | NMIWDRSn | WDRSn | XRSn | POR |
| R-0-0h | W1S-0h | W1S-0h | R-0-0h | W1S-0h | W1S-0h | W1S-0h | W1S-0h |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-12 | RESERVED | R-0 | 0h | Reserved |
| 11 | SIMRESET_XRSn | W1C | 0h | Clear bit for corresponding status bit in RESC. Read of RESCCLR always gives 0. Writing a 1 to this bit clears the status bit in RESC to 0 Writing 0 has no effect. Reset type: SYSRSn |
| 10 | SIMRESET_CPU1RSn | W1C | 0h | Clear bit for corresponding status bit in RESC. Read of RESCCLR always gives 0. Writing a 1 to this bit clears the status bit in RESC to 0 Writing 0 has no effect. Reset type: SYSRSn |
| 9 | RESERVED | R-0 | 0h | Reserved |
| 8 | SCCRESETn | W1S | 0h | Clear bit for corresponding status bit in RESC. Read of RESCCLR always gives 0. Writing a 1 to this bit clears the status bit in RESC to 0 Writing 0 has no effect. Reset type: SYSRSn |
| 7 | RESERVED | R-0 | 0h | Reserved |
| 6 | RESERVED | W1S | 0h | Reserved |
| 5 | RESERVED | W1S | 0h | Reserved |
| 4 | RESERVED | R-0 | 0h | Reserved |
| 3 | NMIWDRSn | W1S | 0h | Clear bit for corresponding status bit in RESC. Read of RESCCLR always gives 0. Writing a 1 to this bit clears the status bit in RESC to 0 Writing 0 has no effect. Reset type: SYSRSn |
| 2 | WDRSn | W1S | 0h | Clear bit for corresponding status bit in RESC. Read of RESCCLR always gives 0. Writing a 1 to this bit clears the status bit in RESC to 0 Writing 0 has no effect. Reset type: SYSRSn |
| 1 | XRSn | W1S | 0h | Clear bit for corresponding status bit in RESC. Read of RESCCLR always gives 0. Writing a 1 to this bit clears the status bit in RESC to 0 Writing 0 has no effect. Reset type: SYSRSn |
| 0 | POR | W1S | 0h | Clear bit for corresponding status bit in RESC. Read of RESCCLR always gives 0. Writing a 1 to this bit clears the status bit in RESC to 0 Writing 0 has no effect. Reset type: SYSRSn |
RESC is shown in Figure 3-60 and described in Table 3-68.
Return to the Summary Table.
Reset Cause register
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| DCON | XRSn_pin_status | RESERVED | |||||
| R-0h | R-X | R-0-0h | |||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | |||||||
| R-0-0h | |||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | SIMRESET_XRSn | SIMRESET_CPU1RSn | RESERVED | SCCRESETn | |||
| R-0-0h | R-0h | R-0h | R-0-0h | R-0h | |||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | RESERVED | RESERVED | RESERVED | NMIWDRSn | WDRSn | XRSn | POR |
| R-0-0h | R-0h | R-0h | R-0-0h | R-0h | R-0h | R-1h | R-1h |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31 | DCON | R | 0h | Reading this bit provides the status of debugger connection to the C28x CPU. 0 : Debugger is not connected to the C28x CPU 1 : Debugger is connected to the C28x CPU Notes: [1] This bit is connected to the DCON o/p signal of the C28x CPU Reset type: N/A |
| 30 | XRSn_pin_status | R | X | Reading this bit provides the current status of the XRSn pin. Reset value is reflective of the pin status. Reset type: N/A |
| 29-16 | RESERVED | R-0 | 0h | Reserved |
| 15-12 | RESERVED | R-0 | 0h | Reserved |
| 11 | SIMRESET_XRSn | R | 0h | If this bit is set, indicates that the device was reset by SIMRESET_XRSn Reset type: PORESETn |
| 10 | SIMRESET_CPU1RSn | R | 0h | If this bit is set, indicates that the device was reset by SIMRESET_CPU1RSn Reset type: PORESETn |
| 9 | RESERVED | R-0 | 0h | Reserved |
| 8 | SCCRESETn | R | 0h | If this bit is set, indicates that the device was reset by SCCRESETn (fired by DCSM). Reset type: PORESETn |
| 7 | RESERVED | R-0 | 0h | Reserved |
| 6 | RESERVED | R | 0h | Reserved |
| 5 | RESERVED | R | 0h | Reserved |
| 4 | RESERVED | R-0 | 0h | Reserved |
| 3 | NMIWDRSn | R | 0h | If this bit is set, indicates that the device was reset by NMIWDRSn. Note: To know the exact cause of NMI after the reset, software needs to read NMISHDFLG registers Reset type: PORESETn |
| 2 | WDRSn | R | 0h | If this bit is set, indicates that the device was reset by WDRSn. Note: [1] A bit inside WD module also provides the same information. This bit is present to keep things consistent. This register is a one-stop shop for the software to know the reset cause for the C28x core. Reset type: PORESETn |
| 1 | XRSn | R | 1h | If this bit is set, indicates that the device was reset by XRSn. Reset type: PORESETn |
| 0 | POR | R | 1h | If this bit is set, indicates that the device was reset by PORn. Reset type: PORESETn |
USER_REG1_SYSRSn is shown in Figure 3-61 and described in Table 3-69.
Return to the Summary Table.
Software Configurable registers reset by SYSRSn
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| BITS | |||||||||||||||||||||||||||||||
| R/W-0h | |||||||||||||||||||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-0 | BITS | R/W | 0h | R/W bits reset by SYSRSn to be used by the application software Reset type: SYSRSn |
USER_REG2_SYSRSn is shown in Figure 3-62 and described in Table 3-70.
Return to the Summary Table.
Software Configurable registers reset by SYSRSn
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| BITS | |||||||||||||||||||||||||||||||
| R/W-0h | |||||||||||||||||||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-0 | BITS | R/W | 0h | R/W bits reset by SYSRSn to be used by the application software Reset type: SYSRSn |
USER_REG1_XRSn is shown in Figure 3-63 and described in Table 3-71.
Return to the Summary Table.
Software Configurable registers reset by XRSn
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| BITS | |||||||||||||||||||||||||||||||
| R/W-0h | |||||||||||||||||||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-0 | BITS | R/W | 0h | R/W bits reset by XRSn to be used by the application software Reset type: XRSn |
USER_REG2_XRSn is shown in Figure 3-64 and described in Table 3-72.
Return to the Summary Table.
Software Configurable registers reset by XRSn
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| BITS | |||||||||||||||||||||||||||||||
| R/W-0h | |||||||||||||||||||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-0 | BITS | R/W | 0h | R/W bits reset by XRSn to be used by the application software Reset type: XRSn |
USER_REG1_PORESETn is shown in Figure 3-65 and described in Table 3-73.
Return to the Summary Table.
Software Configurable registers reset by PORESETn
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| BITS | |||||||||||||||||||||||||||||||
| R/W-0h | |||||||||||||||||||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-0 | BITS | R/W | 0h | R/W bits reset by PORESETn to be used by the application software Reset type: PORESETn |
USER_REG2_PORESETn is shown in Figure 3-66 and described in Table 3-74.
Return to the Summary Table.
Software Configurable registers reset by PORESETn
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| BITS | |||||||||||||||||||||||||||||||
| R/W-0h | |||||||||||||||||||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-0 | BITS | R/W | 0h | R/W bits reset by PORESETn to be used by the application software Reset type: PORESETn |
USER_REG3_PORESETn is shown in Figure 3-67 and described in Table 3-75.
Return to the Summary Table.
Software Configurable registers reset by PORESETn
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| BITS | |||||||||||||||||||||||||||||||
| R/W-0h | |||||||||||||||||||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-0 | BITS | R/W | 0h | R/W bits reset by PORESETn to be used by the application software Reset type: PORESETn |
USER_REG4_PORESETn is shown in Figure 3-68 and described in Table 3-76.
Return to the Summary Table.
Software Configurable registers reset by PORESETn
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| BITS | |||||||||||||||||||||||||||||||
| R/W-0h | |||||||||||||||||||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-0 | BITS | R/W | 0h | R/W bits reset by PORESETn to be used by the application software Reset type: PORESETn |