SPRUJ27C November 2022 – November 2023 TMS320F280033 , TMS320F280034 , TMS320F280034-Q1 , TMS320F280036-Q1 , TMS320F280036C-Q1 , TMS320F280037 , TMS320F280037-Q1 , TMS320F280037C , TMS320F280037C-Q1 , TMS320F280038-Q1 , TMS320F280038C-Q1 , TMS320F280039 , TMS320F280039-Q1 , TMS320F280039C , TMS320F280039C-Q1
Takes ECC address and remaps it to main address space
Synopsis
uint32 Fapi_remapEccAddress(
uint32 u32EccAddress)
Parameters
u32EccAddress [in] | ECC address to remap |
Description
This function returns the main array Flash address for the given Flash ECC address. When the user wants to program ECC data at a known ECC address, this function can be used to obtain the corresponding main array address. Note that the Fapi_issueProgrammingCommand() function needs a main array address and not the ECC address (even for the Fapi_EccOnly mode).
Return Value