SPRZ457J January 2021 – October 2025 AM2431 , AM2432 , AM2434 , AM6411 , AM6412 , AM6421 , AM6422 , AM6441 , AM6442
BCDMA: Blockcopy Gets Corrupted if TR Read Responses Interleave with Source Data Fetch
BCDMA can get corrupted during a block copy operation if the 64B TR descriptor fetch goes to an endpoint that can fragment the 64B burst into smaller burst sizes. This includes DDR where the read transaction will be fragmented to 32B bursts. The only endpoint where fragmentation won't happen is the 2MB OCSRAM. Corruption occurs if the first 32B of the descriptor fetch is returned and the second 32B of the descriptor fetch is delayed such that the BCDMA starts fetching source data and starts receiving that data before the second 32B is received by the BCDMA.
BCDMA block-copy TR descriptors have to be placed in the 2MB OCSRAM. Alternatively the block-copy TR descriptors may be placed in DDR with the requirement that the block copy source data must also be in DDR. Refer to the table below for details.
| Module Endpoint | Size | Could be used for pktDMA descriptors or TR | Could it be used for data buffer for pktDMA( source data or dest data) | Could be used for BCDMA descriptors or TR | BCDMA split TX/RX channel | any considerations on BCDMA source data | Can be used as BCDMA block copy dest data? | PG2.0 Considerations |
|---|---|---|---|---|---|---|---|---|
| DDR | up to 2GB | Yes | Yes | Yes | Yes. Limited to DDR size per TR. no additional TR storage restriction. | Limit to DDR size per TR, and TR for this channel should stored in DDR | Yes, no additional considerations | Yes. Limited to DDR size per TR. No additional TR storage restriction. |
| main R5 TCM | single core mode 64KB ATCM+64KB BTCM. Dual core mode 32KB ATCM+32KB BTCM. | No | Yes | No | Yes, no additional TR storage restriction. | Not to be used as BCDMA's source data | Yes, no additional considerations | Yes, no additional TR storage restriction. |
| main domain on-chip SRAM | 8 banks of memory, each bank is 256KB | Yes | Yes | Yes | Limit to aligned 256KB per TR, can not cross 256KB boundary within the same TR. No additional TR storage considerations. | Limit to aligned 256KB per TR, can not cross 256KB boundary within the same TR. And TR and the source data needs to be in the same memory bank. | Yes, no additional considerations | Limit to aligned 256KB per TR. No additional TR storage requirement. |
| 1KB PSRAM in main_infra | 1KB, used for boot vector storage. Not for TR | No | Yes | No | Limit to aligned 64KB per TR. No additional TR storage considerations. | Not to be used as BCDMA's source data | Yes, no additional considerations | Yes, limited to DMSC_lite memory size (64KB_64KB). no additional TR storage restriction. |
| DMSC_lite SRAM | 64KB+64KB | Yes | Yes | Yes | Yes, no additional TR storage restriction. | Limit to the DMSC_lite memory size (64KB+64KB) per TR. And TR has to be stored in the same memory end point. | Yes, no additional considerations | Yes, limited to DMSC_lite memory size (64KB_64KB). No additional TR storage restriction. |
| OSPI flash | Up to 4GB | No | Yes | No | Yes, no additional TR storage restriction. | Not to be used as BCDMA's source data | Yes, no additional considerations | Yes. Limit to flash size. no additional TR storage restriction. |
| GPMC | up to 128MB | No | Yes | No | Yes, no additional TR storage restriction. | Not to be used as BCDMA's source data | Yes, no additional considerations | Yes. no additional TR storage restriction. |
| PCIe | Up to 4GB | Yes, but Linux does not support this use case | Yes | Yes, but Linux does not support this use case | Yes, no additional TR storage restriction. | The descriptor for Block copy has to be stored on the remote side. Not possible for Linux usecase. | Yes, no additional considerations | Yes. no additional TR storage restriction. |
| ROM | No | Yes, only as source data | No | Only split RX channel. No additional TR storage restriction. | Not to be used as BCDMA's source data | No, ROM only supports read. | Yes. no additional TR storage restriction. |