SPRZ574B December   2023  – October 2025 AM62P , AM62P-Q1

 

  1.   1
  2. 1Usage Notes and Advisories Matrices
    1. 1.1 Devices Supported
  3. 2Silicon Usage Notes and Advisories
    1. 2.1 Silicon Usage Notes
      1.      i2351
      2.      i2424
      3.      i2330
      4.      i2496
    2. 2.2 Silicon Advisories
      1.      i2062
      2.      i2097
      3.      i2103
      4.      i2137
      5.      i2160
      6.      i2189
      7.      i2190
      8.      i2196
      9.      i2208
      10.      i2249
      11.      i2253
      12.      i2278
      13.      i2279
      14.      i2310
      15.      i2311
      16.      i2312
      17.      i2383
      18.      i2401
      19.      i2407
      20.      i2409
      21.      i2410
      22.      i2419
      23.      i2423
      24.      i2431
      25.      i2435
      26.      i2436
      27.      i2457
      28.      i2458
      29.      i2464
      30.      i2482
      31.      i2487
  4.   Trademarks
  5.   Revision History

Usage Notes and Advisories Matrices

Table 1-1 lists all usage notes and the applicable silicon revision(s). Table 1-2 lists all advisories, modules affected, and the applicable silicon revision(s).

Table 1-1 Usage Notes Matrix
MODULE DESCRIPTION SILICON REVISIONS AFFECTED
AM62Px 1.0, AM62Px-Q1 1.0 AM62Px 1.1, AM62Px-Q1 1.1, AM62Px 1.2 AM62Px-Q1 1.2
OSPI i2351 — OSPI: Controller does not support Continuous Read mode with NAND Flash YES YES YES
PLL i2424 — PLL: PLL Programming Sequence May Introduce PLL Instability YES YES YES
DDR i2330 — DDRSS Register Configuration Tool Updates YES YES YES
Package i2496 — Package Pin Assignment Difference between SR1.0/SR1.1 and SR1.2 YES YES YES
Table 1-2 Advisories Matrix
MODULE DESCRIPTION SILICON REVISIONS AFFECTED
AM62Px 1.0, AM62Px-Q1 1.0 AM62Px 1.1, AM62Px-Q1 1.1, AM62Px 1.2 AM62Px-Q1 1.2
BCDMA i2431 — BCDMA: RX Channel can lockup in certain scenarios YES YES YES
BCDMA i2436 — BCDMA: BCDMA RX_IGNORE_LONG setting in RX CHAN CFG register doesn't work YES YES YES
Boot i2410 — Boot: ROM may fail to boot due to i2409 YES NO NO
Boot i2419 — Boot: When disabling deskew calibration, ROM does not check if deskew calibration was enabled YES NO NO
Boot i2423 — Boot: HS-FS ROM applies debug access restrictions to all address space covered by the efuse controller firewall YES NO NO
Boot i2435 — Boot: ROM timeout for eMMC boot too long YES YES YES
Boot i2457 — Boot: Missing data in UART transfer causes boot failures YES NO(1) NO(1)
Boot i2464 — Boot: ROM is unable to boot from SD cards with incorrect formatting YES YES YES
Boot i2482 — Boot: ROM does not provide enough clocks during SD card initialization YES YES YES
CPSW i2208 — CPSW: ALE IET Express Packet Drops YES YES YES
CPSW i2401 — CPSW: Host Timestamps Cause CPSW Port to Lock up YES YES YES
CSI_RX i2190 — CSI_RX_IF may enter unknown state following an incomplete frame YES YES YES
DDR i2160 — DDR: Valid VRef range must be defined during LPDDR4 Command Bus Training YES YES YES
DSS i2097 — DSS: Disabling a layer connected to Overlay may result in synclost during the next frame YES YES YES
Internal Diagnostic Modules i2103 — Incorrect Reporting of ECC_GRP, ECC_BIT and ECC_TYPE Information for Functional Safety Errors YES YES YES
Interrupt Aggregator i2196 — IA: Potential deadlock scenarios in IA YES YES YES
LPM i2487 — LPM: Low power modes may inadvertently corrupt DDR contents YES YES YES
MCAN i2278 — MCAN: Message Transmit order is not ensured from dedicated Tx Buffers configured with same Message ID YES YES YES
MCAN i2279 — MCAN: Specification Update for dedicated Tx Buffers and Tx Queues configured with same Message ID YES YES YES
MMCHS i2312 — MMCHS HS200 and SDR104 Command Timeout Window Too Small YES YES YES
MMCHS i2458 — MMCHS: eMMC HS400 tDCD timing marginal to JEDEC spec YES YES NO
OSPI i2189 — OSPI: Controller PHY Tuning Algorithm YES YES YES
OSPI i2249 — OSPI: Failing OSPI DDR PHY Internal Pad Loopback and No Loopback timing modes YES YES YES
OSPI i2383 — OSPI: 2-byte address is not supported in PHY DDR mode YES YES YES
PRG i2253 —PRG: CTRL_MMR STAT registers are unreliable indicators of POK threshold failure YES YES YES
PSIL i2137 — PSIL: Clock stop operation can result in undefined behavior YES YES YES
RAT i2062 — RAT: Error Interrupt Triggered Even When Error Logging Disable Is Set YES YES YES
RESET i2407— RESET: MCU_RESETSTATz unreliable when MCU_RESETz is asserted low YES YES YES
USART i2310 — USART: Erroneous triggering of timeout interrupt YES YES YES
USART i2311 — USART Spurious DMA Interrupts YES YES YES
USB i2409 — USB: USB2 PHY locks up due to short suspend YES YES YES
See Advisory for important information