SWRU587A November 2021 – March 2023 AWR2944
This is a slider that prompts users to select the desired Maximum Radial Velocity in meters/second. Select the value based on the maximum radial velocity you expect the targets to be moving in within the radar field of view.
Effects on other user knobs
Based on the system resources diverted to fulfill the user-selected value for Maximum Radial Velocity, options for Range Resolution are affected in this configuration.
CLI command details: defines the number of loops in the frameCfg command.