DLPS167A March 2024 – September 2024 DLPC964
PRODUCTION DATA
All register addresses are 32-bit in size, where each register contains a 32-bit value. The actual valid bits are shown in each respective register. Most registers contain spare or unused bits. These bits must be treated as don't-care during a read operation unless otherwise specified. When writing to spare or unused bits, these bits MUST be set to 0. Both the register address and the data require the least-significant byte to be first and most-significant byte last. A SUB CMD must precede the register address to indicate the type of operation; whereas 0xF1 indicates a write operation and a 0xF2 indicates a read operation. The following figures show examples of writing and reading to the DESTOP_BUS_SWAP register.
Figure 6-2 shows an I2C primary writing data to the DLPC964, where 0xF1 is required as the SUB CMD followed by the register address and finally the register data.
Figure 6-3 shows an I2C primary reading data from the DLPC964, where 0xF2 is required as the SUB CMD followed by the register address. Then the primary performs STOP followed by a START to read the register data.