DLPU018J October 2014 – June 2024 DLPC900
To execute a command to set the Input Data Channel Swap value, the host builds a sequence of bytes containing the Secondary address, the sub-address, and the data, and performs the following steps.
An example of the above write command sequence is shown in Table 1-4, and a waveform diagram of a host executing this write sequence is shown in Figure 1-3.
| SECONDARY ADDRESS | SUB-ADDRESS | DATA | |||
|---|---|---|---|---|---|
| 0x34 | 0x84 | 0x02 | |||
Figure 1-3 I2C Write Command Waveform
Diagram