DLPU082B August 2021 – August 2022 DLPC7540
While writing to the DLPC operating in the I2C target configuration, the first byte following the start condition should be the DLPC device write address (34h). It is possible to change the device address to any other desired value using DLP Composer tool. The remaining bytes are sent as specified in the command protocol section Section 16.
While reading from the DLPC in I2C target configuration, the first byte following the start condition should be DLPC device write address +1 (35h default) followed by header and opcode bytes as explained later in the document. All reads from DLPC via I2C interface starts with a write as explained above specifying the opcode for read. The host should then continue the I2C transaction with a Restart-Read followed by the number of bytes associated with the command and finally the Stop.