DLPU114A August 2024 – November 2024 DLPC8445
| Set Blendmap Gain Values | |
|---|---|
| Write Parameter(s) | |
| Byte | Description |
| Byte 0 |
Color Channel Select 0 = Green color 1 = Red color 2 = Blue color |
| Bytes 1-2 |
Start index in the table for the data to be written |
| Bytes 3 - * |
Gain of control points .The format of input should be such that required gain which is a value between 0 to 1.99 be multiplied by 4096 before passing it in command. |