SBAA264B January 2018 – September 2024 ADS7044 , ADS7047 , ADS7054 , ADS7057
| Input | ADC Input | Digital Output ADS7057 |
|---|---|---|
| Vin Min = –3.3V | AINP = 0V AINM = 3.3V |
2000H 819210 |
| Vin Max = 3.3V | AINP = 3.3V AINM = 0V |
1FFFH 819110 |
| AVDD | GND | DVDD |
|---|---|---|
| 3.3V | 0V | 1.8V |
This design is intended to demonstrate how to convert a unipolar, single-ended signal into a unipolar, fully-differential signal and drive a differential ADC (for more information on these and other signal types, please refer to the TI Precision Labs training titled SAR ADC Input Types). Compared to a single-ended device, a fully-differential ADC has twice the dynamic range which improves the AC performance of the converter. Many common systems, for example Sonar Receivers, Flow Meters, and Motor Controls, benefit from the higher performance of a differential ADC. The equations and explanation of component selection in this design can be customized based on system specifications and needs. For more information on a similar design using a bipolar input, see the cookbook circuit titled Single-Ended to Differential Using an Op Amp and FDA for Bipolar Signals.
| Specification | Calculated | Simulated |
|---|---|---|
| Transient ADC Input Settling (at 250ksps) | < 0.5 × LSB = 201µV | 144.8µV |
| Conditioned Signal Range (at 250ksps) | > 99% ADC FSR = > 6.53V | 6.60V |
| Noise | 43.8µV ÷ √Hz | 44.3µV ÷ √Hz |





The operational amplifier is used to protect the sensor from any charge kickbacks that occur when the ADC connects or disconnects the sampling capacitor. This amplifier may not be needed if the sensor has a high-output impedance. A negative rail is used for both the OPA320 and THS4551 based on the assumption that the sensor is operating with a negative rail; this also provides the highest performance from the ADC by providing the full scale input range.
The following graph shows the simulated output for a 0 - 3.3V input. The analog front end has a linear output of ±3.3V which matches the full-scale range (FSR) of the ADC (with AVDD = 3.3V).
The bandwidth of the analog front end is simulated to be 4.12MHz at the gain of 0dB which is a linear gain of 1. This bandwidth allows the inputs of the ADC to adequately settle for a 250-ksps input signal.
The following simulation shows the ADC sample and hold capacitor settling for a 3.3-V DC input signal. This simulation shows that the analog front end is able to drive the ADC with a large step input (from 0V to 3.3V) so it settles to within ½ of an LSB (approximately 200µV) in the allotted acquisition time (95ns). Refer to Introduction to SAR ADC Front-End Component Selection for detailed theory on this subject, and follow the link at the end of this design to download these simulation files.
This section walks through a simplified noise calculation, providing a rough estimate to compare with the simulated result. The resistor noise is included in this calculation as it is a significant portion of the overall noise of the system. Note that the resistor noise can be reduced by using smaller value resistors, but at the expense of increased power consumption through the feedback network.

Note that calculated and simulated match well. Refer to the TI Precision Labs - ADCs training video series for detailed theory on this subject.
| Device | Key Features | Link | Similar Devices |
|---|---|---|---|
| ADS7057 | 14 bit, 2.5 Msps, fully-differential input, SPI, 2.25mm2 package | 14-Bit, 2.5MSPS, Differential Input, Small-Size Low-Power SAR ADC | Precision ADCs |
| THS4551 | 150MHz, 3.3nV/√Hz input voltage noise, fully-differential amplifier | Low Noise, Precision, 150MHz, Fully Differential Amplifier | Fully differential amplifiers |
| OPA320 | Precision, zero-crossover, 20MHz, 0.9pA Ib, RRIO, operational amplifier | Precision, zero-crossover, 20MHz, 0.9pA Ib, RRIO, CMOS operational amplifier | Operational amplifiers (op amps) |
The ADS7057 uses the AVDD as the reference input. Use a high-PSRR LDO, such as the TPS7A47, as the power supply.
Texas Instruments, design files for SBAA264, SBAC188 software support