SBAA438A June 2020 – March 2023 AMC1100 , AMC1200 , AMC1300B-Q1 , AMC1302 , AMC1311 , AMC1336 , AMC3301 , AMC3330 , ISO224
Released in 2018, the ISO224 closely managed the energy crossing over the isolation barrier, and added OOK data transmission. The radiated emissions EMI scan shown in Figure 3-1 was performed using the ISO224 and the emissions are first seen around 540 Mhz with 18 dB of margin and continues to 1 GHz which is the CISPR 11 test limit, with 6 dB of margin at 940 MHz.
Texas Instruments released the AMC1100 and AMC1200 isolated amplifiers in 2011. These devices feature a basic isolation barrier and meet the CISPR 11 Class A and Class B standards with sufficient margin.
As shown in Figure 3-2, the AMC1200 has several radiated emissions peaks above the noise floor, however, there is a significant amount of margin available to the CISPR class B limit shown in black. The noise peaks in the 100 MHz to 230 MHz region have 24 dB of margin from the CISPR11 Class B limit, while the noise peaks in the higher frequency range, 480 MHz to 630 MHz, have 13 dB of margin.
Figure 3-2 AMC1200 CISPR 11 Radiated Emissions EMI Scan