SBAA767 January 2026 OPA206
In frequency response of a standard second order system, a resonance exists only if ζ<1/√2. The resonant peak, Mr, at the resonant frequency is given by:
Figure 4-4 Gain PeakingSolvingEquation 49 for ζ yields Equation 50.
Let ζ2 be y. Then, Equation 50 can be written as:
Solving for y yields:
Since the range of ζ<1/√2 is assumed, take the smaller value.
By substituting Equation 54 into Equation 46
From Equation 55, Figure 4-5 can be drawn.
Figure 4-5 Phase Margin vs Gain
PeakingTable 4-2 lists some examples of an expected ac-gain peaking at each phase margin.
| Phase Margin | Gain Peaking |
|---|---|
| 15° | 11.7dB |
| 30° | 5.7dB |
| 45° | 2.3dB |
| 60° | 0.28dB |