SBAA767 January   2026 OPA206

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2General Transfer Function of the Second Order System
    1. 2.1 Damping Ratio
      1. 2.1.1 Underdamped (0 < ζ < 1)
      2. 2.1.2 Critically Damped (ζ = 1)
      3. 2.1.3 Overdamped (ζ>1)
  6. 3Modeling Op-Amp as a Second Order System
  7. 4Phase Margin vs Percent Overshoot
    1. 4.1 Phase Margin
    2. 4.2 Represent AOLβ as ΦPM
    3. 4.3 Represent ΦPM as Damping ratio
    4. 4.4 Phase Margin Represented by Percent Overshoot
    5. 4.5 Phase Margin Represented by Gain Peaking
  8. 5Simulation of Ideal Second Order System
    1. 5.1 Phase Margin: 30 Degrees
    2. 5.2 Phase Margin: 45 Degrees
    3. 5.3 Phase Margin: 60 Degrees
    4. 5.4 Phase Margin: 75 Degrees
    5. 5.5 Step Response with Different Phase Margin (Damping Ratio)
    6. 5.6 Gain Peaking with Different Phase Margin (Damping Ratio)
  9. 6Simulation Example Using an Op-Amp
    1. 6.1 OPA392 With Non-Inverting Amp Configuration
      1. 6.1.1 Step Response Simulation
      2. 6.1.2 Gain Peaking Simulation
      3. 6.1.3 Loop Gain Simulation
    2. 6.2 TLV9052 with Unity Gain Buffer Configuration
      1. 6.2.1 Step Response Simulation
      2. 6.2.2 Gain Peaking Simulation
      3. 6.2.3 Loop Gain Simulation
    3. 6.3 OPA206 with Unity Gain Buffer Configuration
      1. 6.3.1 Step Response Simulation
      2. 6.3.2 Gain Peaking Simulation
      3. 6.3.3 Loop Gain Simulation
  10. 7Causes of the Mismatch of Phase Margin Between Step Response and AC Analysis
    1. 7.1 The Transfer Function is not a Second Order System
    2. 7.2 Amplifier Showing Large-Signal Behavior
    3. 7.3 Noise Gain is Not Flat Within Crossover Frequency
  11. 8Summary
  12. 9References

Phase Margin

Phase margin ΦPM is calculated as the difference between the phase shift of the system at the crossover frequency, ωC and 180 degrees. In a second order system, phase lag is caused by the first pole, ωp1 and the second pole, ωp2 as shown in Figure 4-1.

グラフ AI 生成コンテンツは誤りを含む可能性があります。 Figure 4-1 Phase Margin of a Second Order System

In general, the first pole is located at much lower than crossover frequency, leading to 90 degrees (=π/2) lag.

An equation of the second pole is given by:

Equation 20. 1 1 + ω ω p 2 j = 1 1 + ω ω p 2 2 - ω ω p 2 1 + ω ω p 2 2 j
ダイアグラム AI 生成コンテンツは誤りを含む可能性があります。 Figure 4-2 Phase Lag of the Second Pole

As shown in Figure 4-2, the phase shift of the second pole can be calculated as follows.

Equation 21. tan θ = - ω ω p 2 1 + ω ω p 2 2 1 1 + ω ω p 2 2
Equation 22. = - ω ω p 2
Equation 23. θ = tan - 1 ⁡ - ω ω p 2
Equation 24. = - tan - 1 ⁡ ω ω p 2

At crossover frequency, ωC where magnitude of loop gain is equal to 1, the phase shift by the second pole becomes below from Equation 24.

Equation 25. - tan - 1 ⁡ ω c ω p 2

The total phase shift at crossover frequency due to first pole and second pole can be calculated as

Equation 26. - π 2 - tan - 1 ⁡ ω c ω p 2

Calculation of difference between π and Equation 26 yields phase margin.

Equation 27. ϕ P M = π - π 2 - tan - 1 ⁡ ω c ω p 2
Equation 28. = π 2 - tan - 1 ⁡ ω c ω p 2