A data transfer frame between the device and the host controller is bounded between a
CS falling edge and the subsequent
CS rising edge. The host controller can initiate a data transfer frame (as shown in Figure 6-11) at any time irrespective of the status of the CONVST signal; however, the data read during such a data transfer frame is a function of relative timing between the CONVST and
CS signals.
For this discussion, assume that the CONVST signal remains low.
For a typical data transfer frame F:
- The host controller pulls
CS low to initiate a data transfer frame. On the
CS falling edge:
- RVS goes low, indicating the beginning of the data transfer frame.
- The SCLK counter is reset to 0.
- The device takes control of the data bus. As shown in Figure 6-11, the 20-bit contents of the output data word (see Figure 6-9) are loaded in to the 20-bit ODR (see Figure 6-5).
- The 20-bit IDR (see Figure 6-5) is reset to 00000h, corresponding to a NOP command.
- During the frame, the host controller provides clocks on the SCLK pin:
- On each SCLK capture edge, the SCLK counter is incremented and the data bit received on the SDI pin is shifted in to the IDR.
- On each launch edge of the output clock (SCLK in this case), ODR data are shifted out on the selected SDO-x pins.
- The status of the RVS pin depends on the output
protocol selection (see the Protocols for Reading From the Device section).
- The host controller pulls
CS high to end the data transfer frame. On the
CS rising edge:
- The SDO-x pins go to tri-state.
- RVS goes high (after a delay of td_RVS).
- As illustrated in Figure 6-11, the 20-bit contents of the IDR are transferred to the command processor (see Figure 6-5) for decoding and further action.
After pulling CS high, the
host controller must monitor for a low-to-high transition on the RVS pin or wait for the
td_RVS time (see the Timing Requirements: SPI-Compatible Serial Interface table) to elapse before
initiating a new operation (data transfer or conversion). The delay, td_RVS, for
any data transfer frame F varies based on the data transfer operation executed in the frame
F.
At the end of the data transfer frame F:
- If the SCLK counter is < 20, it indicates that IDR has captured less than 20 bits from the SDI. In this case, the device treats the frame F as a short command frame. At the end of a short command frame, the IDR is not updated and the device treats the frame as a no operation command.
- If the SCLK counter = 20, it indicates that the IDR has captured exactly 20 bits from SDI. In this case, the device treats the frame F as a optimal command frame. At the end of an optimal command frame, the command processor decodes the 20-bit contents of the IDR as a valid command word.
- If the SCLK counter > 20, it indicates that the IDR captured more than 20 bits from the SDI, and only the last 20 bits are retained. In this case, the device treats the frame F as a long command frame. At the end of a long command frame, the command processor treats the 20-bit contents of the IDR as a valid command word. There is no restriction on the maximum number of clocks that can be provided within any data transfer frame F. However, as explained above, the last 20 bits shifted into the device prior to the
CS rising edge must constitute the desired command.
In a short command frame, the write operation to
the device is invalidated, however, the output data bits transferred during the frame are
still valid output data. Therefore, the host controller can use such shorter data transfer
frames to read only the required number of MSB bits from the 20-bit output data word. As
shown in Figure 6-9, an optimal read frame for ADS9110 needs to read only the 18 MSB bits
of the output data word. The length of an optimal read frame depends on the output protocol
selection; refer to the Protocols for Reading From the Device section for more details.
Note: The example above shows data read and data write operations synchronous to the external clock provided on the SCLK pin.
The device also supports data read operation
synchronous to the internal clock; see the Protocols for Reading From the Device section for more details. In this
case, while the ODR contents are shifted on the SDO(s) on the launch edge of the internal
clock, the device continues to capture the SDI data into IDR (and increment the SCLK
counter) on SCLK capture edges.