Selection criteria for the input amplifiers is highly dependent on the input signal type, as well as the performance goals, of the data acquisition system. Some key amplifier specifications to consider when selecting an appropriate amplifier to drive the inputs of the ADC are:
- Small-signal bandwidth. Select the
small-signal bandwidth of the input amplifiers to be as high as possible after
meeting the power budget of the system. Higher bandwidth reduces the closed-loop
output impedance of the amplifier, thus allowing the amplifier to more easily
drive the ADC sample-and-hold capacitor and the RC filter (Charge-Kickback Filter) at the inputs of the ADC. Higher bandwidth
amplifiers offer faster settling times while driving the capacitive load of the
charge-kickback filter, thus reducing harmonic distortion at higher input
frequencies. To maintain the overall stability of the input driver circuit,
select the amplifier with a unity gain bandwidth (UGB) as described in Equation 17:
Equation 17.
- Distortion. Both the ADC and the input
driver introduce distortion in a data acquisition block. To make sure that the
distortion performance of the data acquisition system is not limited by the
front-end circuit, the distortion of the input driver must be at least 10dB less
than the distortion of the ADC, as shown in Equation 18.
Equation 18.
- Noise. Noise contribution of the front-end
amplifiers must be as low as possible to prevent any degradation in SNR
performance of the system. Generally, to make sure that the noise performance of
the data acquisition system is not limited by the front-end circuit, the total
noise contribution from the front-end circuit must be kept below 20% of the
input-referred noise of the ADC. Noise from the input driver circuit is
band-limited by designing a low cutoff frequency, charge-kickback filter, as
explained in Equation 19.
Equation 19.
where:
- V1 / f_AMP_PP
is the peak-to-peak flicker noise in µV
- en_RMS is the
amplifier broadband noise density in nV/√ Hz
- f–3dB is the
3dB bandwidth of the charge-kickback filter
- NG is the
noise gain of the front-end circuit that is equal to 1 in a buffer
configuration
- Settling Time. For dc signals with fast
transients that are common in a multiplexed application, the input signal must
settle within an 16-bit accuracy at the device inputs
during the acquisition time window. This condition is critical to maintain the
overall linearity performance of the ADC. Typically, amplifier datasheets
specify the output settling performance only up to 0.1% to 0.001%, which is not
always sufficient for the desired 16-bit accuracy. Therefore, always verify
the settling behavior of the input driver by TINA-TI SPICE simulations before
selecting the amplifier.